Hi,
I have a problem with transferring data from a Stellaris ARM CPU to the 21469 over SPI. The DSP is configured as slave.
I can successfully boot the DSP as a slave from the CPU, so in principle, the connection works fine.
However, normal data transfer after booting the DSP does not work.
I boiled down my code to a small test program just to check SPI.
Here it is
/***************************************************************************** * main.c *****************************************************************************/ #include <sysreg.h> #include "defines.h" #include <sru21469.h> #include<cs_macros.h> void Receive_data(int i); int destination[16]; int dma_done = 0; void main() { ADSP_2146X_PLL_Init_INDIV_STEP_NOT_REQUIRED(36,2,0,2,3); *pSPICTL = 0; *pSPIDMAC = 0; *pSPIBAUD = 0; *pSPIFLG = 0; interrupt(SIG_SPIH, Receive_data); *pIISPI = (int)destination; *pIMSPI = 1; *pCSPI = 16; *pSPICTL = RXFLSH | TXFLSH; *pSPIDMAC = FIFOFLSH; *pSPICTL = MSBF| CPHASE| CLKPL| SPIEN | WL16 | TIMOD2 ; *pSPIDMAC = SPIDEN | SPIRCV | INTEN; while(1) { asm("nop;"); } } void Receive_data(int i) { dma_done = 1; }
From the CPU, I send data by manually controlling the slave select line to be able to control the timing in detail.
With a scope, I recorded the signals data, clk, slave select (from top to bottom),
I don't see anything wrong with this, however, the data are not transferred.
The weirdest thing is, that yesterday, 3 or 4 times it worked, today, I can not reproduce that. Booting over SPI still works.
SPI rate is 50kHz, currently, but I also tested values up to 500kHz.
What do I miss?
Regards,
Rainer
The issue is solved. The board seems to have a failure. Using a different board works fine.