Post Go back to editing

talkthrough example on ADSP21369 with AD1835 in TDM mode

Hi,

I am trying to implement talkthrough example on ADSP21369 with AD1835 codec in TDM mode (8in/8out). I don't know how to configure AD1835 in TDM mode.

Can anyone send me the example code which is working on ADSP21369 with AD1835 in TDM mode?

Best Regards,

Madhan

Parents
  • Hi Madhan,

    In order to implement a talk through code for ADSP-21369 processor, you need to configure the codec (AD1835) to support TDM mode and the SPORT [in the existing talk through example code for ADSP-21369] .

    I am attaching a simple code which configures the SPORT in TDM mode for a reference.

    You would also like to go through the example codes of ADSP-21469 processor as well. Though the codec there is AD1939, but it will give an insight as where and what all changes you will have to make for ADSP-21369 example code to support TDM mode. The example codes for ADSP-21469 is available in the following path:

    …\Program Files (x86)\Analog Devices\VisualDSP 5.0\214xx\Examples\ADSP-21469 EZ-Board

    For more information regarding AD1835, kindly refer to its datasheet, the link for which is given below:

    http://www.analog.com/static/imported-files/data_sheets/AD1835.pdf

    Please let me know in case you have any further queries/doubts.

    Thanks,

    Harshit

    SPORT_TDM_mode.zip
Reply
  • Hi Madhan,

    In order to implement a talk through code for ADSP-21369 processor, you need to configure the codec (AD1835) to support TDM mode and the SPORT [in the existing talk through example code for ADSP-21369] .

    I am attaching a simple code which configures the SPORT in TDM mode for a reference.

    You would also like to go through the example codes of ADSP-21469 processor as well. Though the codec there is AD1939, but it will give an insight as where and what all changes you will have to make for ADSP-21369 example code to support TDM mode. The example codes for ADSP-21469 is available in the following path:

    …\Program Files (x86)\Analog Devices\VisualDSP 5.0\214xx\Examples\ADSP-21469 EZ-Board

    For more information regarding AD1835, kindly refer to its datasheet, the link for which is given below:

    http://www.analog.com/static/imported-files/data_sheets/AD1835.pdf

    Please let me know in case you have any further queries/doubts.

    Thanks,

    Harshit

    SPORT_TDM_mode.zip
Children
No Data