Re: HDMI input via ADV7622 into ADSP 21489

Hi,

I'm using an ADSP 21489 attached to the EZ extender, along with an ADV 7623 for HDMI input. Where can I find some sample code to get HDMI input into the ADSP 21489, and get analog out via the EZ Extender?

Regards,

Naveen

Parents
  • 0
    •  Analog Employees 
    on Jul 16, 2013 12:20 AM

    Hi Naveen,

    I’ll try to explain the use of TCB and the chain pointer register.

    With chained DMA, the attributes of a specific DMA are stored in internal memory and are referred to as a Transfer Control Block or TCB. The location of the DMA parameters for the next sequence comes from the chain pointer register that points to the next set of DMA parameters stored in the processor’s internal memory. The processor automatically initializes and then begins another DMA transfer when the current DMA transfer is complete. Each new set of parameters is stored in a user-initialized memory buffer or TCB

    Each SPORT DMA channel has a chain pointer register (CPSPxy). In chained DMA operations, the processor’s DMA controller automatically sets up another DMA transfer when the contents of the current buffer have been transmitted (or received). The chain pointer register (CPSPxy) functions as a pointer to the next set of buffer parameters stored in external or internal memory. The DMA controller automatically downloads these buffer parameters to set up the next DMA sequence.

    Thanks,

    Mahesh

Reply
  • 0
    •  Analog Employees 
    on Jul 16, 2013 12:20 AM

    Hi Naveen,

    I’ll try to explain the use of TCB and the chain pointer register.

    With chained DMA, the attributes of a specific DMA are stored in internal memory and are referred to as a Transfer Control Block or TCB. The location of the DMA parameters for the next sequence comes from the chain pointer register that points to the next set of DMA parameters stored in the processor’s internal memory. The processor automatically initializes and then begins another DMA transfer when the current DMA transfer is complete. Each new set of parameters is stored in a user-initialized memory buffer or TCB

    Each SPORT DMA channel has a chain pointer register (CPSPxy). In chained DMA operations, the processor’s DMA controller automatically sets up another DMA transfer when the contents of the current buffer have been transmitted (or received). The chain pointer register (CPSPxy) functions as a pointer to the next set of buffer parameters stored in external or internal memory. The DMA controller automatically downloads these buffer parameters to set up the next DMA sequence.

    Thanks,

    Mahesh

Children
No Data