Re: HDMI input via ADV7622 into ADSP 21489

Hi,

I'm using an ADSP 21489 attached to the EZ extender, along with an ADV 7623 for HDMI input. Where can I find some sample code to get HDMI input into the ADSP 21489, and get analog out via the EZ Extender?

Regards,

Naveen

Parents
  • Hi Mahesh,

    There is just one standard way of making that interface - The ADV7623 along with a HDMI adapter board is connected to the EZ Extender.

    How exactly is *pCPSP4A related to SPORT 4A? If I have the address of a transfer control buffer in *pCPSP4A, how could I get the data in SPORT 4A to the transfer control buffer?

    Thanks,

    Naveen

Reply
  • Hi Mahesh,

    There is just one standard way of making that interface - The ADV7623 along with a HDMI adapter board is connected to the EZ Extender.

    How exactly is *pCPSP4A related to SPORT 4A? If I have the address of a transfer control buffer in *pCPSP4A, how could I get the data in SPORT 4A to the transfer control buffer?

    Thanks,

    Naveen

Children
No Data