Post Go back to editing

twi interfacing problem....

Hi,

i am using AD7415 temperature sensor in floating mode of AS. i followed the instructions as per the hard ware reference to interface  an i2c device(AD7415). but it was not generating clock. following attachment consists C code. i am using core clock frequency of 200MHz.

trail1.c.zip
Parents
  • Hi Durga,

    There is an example C code in VDSP installation folder (..\Analog Devices\VisualDSP 5.0\214xx\Examples\ADSP-21479 EZ-Board\Power_On_Self_Test\ temp_sensor_test.c ) which demonstrates the Temperature sensor (ADM1032) interfaced to Sharc through TWI interface(master). You can go through the same for your reference.

    Regards,

    Mahesh

Reply
  • Hi Durga,

    There is an example C code in VDSP installation folder (..\Analog Devices\VisualDSP 5.0\214xx\Examples\ADSP-21479 EZ-Board\Power_On_Self_Test\ temp_sensor_test.c ) which demonstrates the Temperature sensor (ADM1032) interfaced to Sharc through TWI interface(master). You can go through the same for your reference.

    Regards,

    Mahesh

Children
No Data