Post Go back to editing

Help on ADSP-21489 firmware update via RS-232

Hi,

We are looking for some assistance with adding the ability to update our

ADSP-21489 firmware via RS-232. The fundamentals of what we want to do is

discussed in Application Note EE-345, and we have played around with this a

little bit, but never got it to work completely. We can continue to puzzle

through this ourselves, but we'd rather find a consultant who can help add

this ability into our existing software and we'll be happy to pay someone to

help in this regard.

If you have experience in this area and have some extra time on your hands,

and want to earn some extra money in your pocket, please contact me.

(Ideally the forum has some private messaging system, otherwise you could

leave an email address. Let me know your thoughts...)

Thank you,

Marc

Parents
  • Hi Harshit,

    Actually, we are trying to do this firmware upgrade through UART for serial Flash on the ADSP-21489.

    We have made a custom board with the ADSP-21489 and the code is loaded on the Flash M25P16. We have loaded it through the Flash programming to on VisualDSP++.

    Now, the goal is to upgrade this flash memory through UART, because there will be a software which communicates with the board and allows to update the firmware if available.

    The Application Note EE-345 provides example for ADSP-21469. I saw all the threads concerning migration  to ADSP-21489 but I didn't get a clear example or explanation.

    I don't know what to modify to get it work on ADSP-21489. This thread provides an example (http://ez.analog.com/message/59942#59942) but for Parallel upgrade.

    This application note has been released on October 2009. Is there any update of this application note that could provide an example for ADSP-21489?

    I would really appreciate your help on this,

    Best regards,
    Marc

Reply
  • Hi Harshit,

    Actually, we are trying to do this firmware upgrade through UART for serial Flash on the ADSP-21489.

    We have made a custom board with the ADSP-21489 and the code is loaded on the Flash M25P16. We have loaded it through the Flash programming to on VisualDSP++.

    Now, the goal is to upgrade this flash memory through UART, because there will be a software which communicates with the board and allows to update the firmware if available.

    The Application Note EE-345 provides example for ADSP-21469. I saw all the threads concerning migration  to ADSP-21489 but I didn't get a clear example or explanation.

    I don't know what to modify to get it work on ADSP-21489. This thread provides an example (http://ez.analog.com/message/59942#59942) but for Parallel upgrade.

    This application note has been released on October 2009. Is there any update of this application note that could provide an example for ADSP-21489?

    I would really appreciate your help on this,

    Best regards,
    Marc

Children
No Data