Post Go back to editing

Why is there such a long delay in Talkthru Analog In-Out?

Thread Summary

The user observed a 1.3ms delay between input and output signals on the ADZS-21369-EZLITE using the Talktru Analog In-Out example program. The delay is primarily due to the AD1835 Codec's built-in decimation and interpolation filters. Increasing the sampling rate to 192 kHz can halve the group delay.
AI Generated Content

I started with the Talktru Analog In-Out example program using an ADZS-21369-EZLITE.  I slightly rewrote the program so I could get data in and out of my program.  When I ran the program I noticed about a 60 sample delay between the input and output.  I assume the example program has the same delay.  I finally reduced my interrupt routine to the program below.  I took a sine wave and split it into RXSP0A and a scope and then took the signal from TXSP1B into the other channel of the scope.  I find about a 1.3ms delay between the two scope waveforms.  Is there someway to configure the SPORT to reduce this?  Do I need to use DMA?  Which manual applies to the 21369, the "2136x SHARC Processor Hardware Reference" manual doesn't include the 21369?

Hal

.section /pm seg_pmco;

.global _talkThroughISR;

_talkThroughISR:

       HLoop: r14=r14 XOR r15;

    if EQ JUMP HRight;

   

r10=dm(RXSP0A);          // Read new left sample from ADC

          r13=LSHIFT r10 BY 0x08;

f13=FLOAT r13;

dm(TXSP1B)=r10; //to scope channel

     

rti;

HRight: 

         r10=0;

        

dm(TXSP1B)=r10;

r10=dm(RXSP0A);    //dummy read 

rti;

///////////////////////////////////////////////////////////////////////////////////////////////

//NAME:     main.asm                                                                         //

//DATE:     7/29/05                                                                          //

//PURPOSE:  ADSP-21369 EZ-KIT Test. Calls initialization routines then waits for interrupts  //

//                                                                                           //

//USAGE:    This file contains the main routine calls functions to set up the talkthrough    //

//          routine. It receives an input signal from the ADC via SPORT0A and outputs to     //

//          DAC's via SPORT1A, SPORT1B, SPORT2A, and SPORT2B.                                //

//                                                                                           //

///////////////////////////////////////////////////////////////////////////////////////////////

#include <def21369.h>

#include "btc.h"   //BTC channel to observe variables

.section /pm seg_pmco;

.global _main;

.extern _initPLL;

.extern _initSDRAM;

.extern _initSRU;

.extern _initSPORT;

.extern _init1835viaSPI;

.extern _initMLS;

.extern _initFIR;

_main:

    call _initPLL;        // Initializes PLL for the correct core clock (CCLK) frequency

    call _initSDRAM;      // Initializes SDRAM for the correct SDRAM clock (SDCLK) frequency

    call _initSRU;        // Initializes the SRU & DAI/DPI pins

    call _init1835viaSPI; // Initializes the codec

   

    call _initMLS;       //  Initialize MLS sequence generator

   

    call _initFIR;          //  Initialize  FIR  

    call _initSPORT;      // Initializes the transmit and receive serial ports (SPORTS)

   

//-----------------------------------------------------------------

    // Enable interrupts (globally)

    BIT SET MODE1 IRPTEN;

    //----------------------------------------------------------------

    // Unmask the SPORT0 ISR

    LIRPTL = SP0IMSK;

_main.end:

    //----------------------------------------------------------------

    // Loop forever.  Work is driven by interrupts

    jump (pc,0);

init1835viaSPI.asm

#include <def21369.h>

#include "ad1835.h"

.global _init1835viaSPI;

//===============================================================

.section/dm seg_dmda;

.var spi_semaphore;

.var config_tx_buf[]=          // Buffer of configuration data

            WR | DACCTRL1 | DACI2S | DAC24BIT | DACFS48,

            WR | DACCTRL2, // e.g.: | DACMUTE_R1 | DACMUTE_L2,

            WR | DACVOL_L1 | DACVOL_MAX,

            WR | DACVOL_R1 | DACVOL_MAX,

            WR | DACVOL_L2 | DACVOL_MAX,

            WR | DACVOL_R2 | DACVOL_MAX,

            WR | DACVOL_L3 | DACVOL_MAX,

            WR | DACVOL_R3 | DACVOL_MAX,

            WR | DACVOL_L4 | DACVOL_MAX,

            WR | DACVOL_R4 | DACVOL_MAX,

            WR | ADCCTRL1 | ADCFS48,

            WR | ADCCTRL2 | ADCI2S | ADC24BIT,

            WR | ADCCTRL3 | IMCLKx2 | PEAKRDEN;

//===============================================================

.section/pm seg_pmco;

_init1835viaSPI:

    //--------------------------

    // Clear SPTFLG and SPICTL regs to start

    r0 = 0;

    dm(SPICTL)=r0;

    dm(SPIFLG)=r0;

    //---------------------------------------------------------

    // Writing TXFLSH and RXFLSH bits in SPICTL clear the SPI

    // transmit and receive FIFOs, respectively.

    r0 = dm(SPICTL);

    r1 = (TXFLSH | RXFLSH );

    r0 = r0 OR r1;

    dm(SPICTL)=r0;

    //----------------------------

    // Setup the baud rate to 500 KHz

    r0 = 100;

    dm(SPIBAUD) = r0;

    //--------------------------------------------

    // Set the SPIFLG register to FLAG3 (0xF708)

    r0 = 0xF708;

    dm(SPIFLG) = r0;

    //------------------------------------------------------

    // Now set the SPI control register

    r0 = (SPIEN |   // enable the port

          SPIMS |   // set SHARC as SPI master

          MSBF |    // send MSB first

          WL16 |    // word length = 16 bits

          TIMOD1);  // Initialize SPI port to begin

                    // transmitting when DMA is enabled

    dm(SPICTL) = r0;

    //-------------------------------------------

    // Set up DAG registers to transmit via SPI

    i4 = config_tx_buf;

    m4 = 1;

    //------------------------------

    // Set up loop to transmit data

    lcntr = LENGTH(config_tx_buf), do word_sent until lce;

        // Send a word

        r0=dm(i4,m4);

        dm(TXSPI)=r0;

        // Wait until "SPI transfer complete" status bit

        //   in SPISTAT (SPIFE) indicates that we can send more

        do checkIfTXisDone until TF;

            ustat3 = dm(SPISTAT);

            BIT TST ustat3 SPIFE;

        checkIfTXisDone:

        nop;

        // Wait an extra 100 cycles to meet the timing

        //   requirements of the AD1835A

        lcntr = 100, do pauseFor1835 until lce;

        pauseFor1835:

        nop;

    word_sent:

    nop;

/*

    //-----------------------------------------

    // Flush SPI buffers after initialization

    //   You may want to do this before sending

    //   other SPI commands to guarantee that

    //   you have not accidentally left data in

    //   the transmit or receive FIFOs.

    r0 = dm(SPICTL);

    r1 = (TXFLSH | RXFLSH );

    r0 = r0 OR r1;

    dm(SPICTL)=r0;

*/

_init1835viaSPI.end:

    rts;

////////////////////////////////////////////////////////////////////////////////////////////

//NAME:     initSPORT.asm

//DATE:     7/29/05

//USAGE:    This file initializes the transmit and receive serial ports (SPORTS). It uses

//               uses SPORT0 to receive data from the ADC and transmits the data to the DAC's

//               via SPORT1A, SPORT1B, SPORT2A and SPORT2B.

//

////////////////////////////////////////////////////////////////////////////////////////////

#include <def21369.h>

#include <Main.h>

.global _initSPORT;

.extern H;

.extern HCount;

.extern HiCount;

.extern HirCount;

.extern Mike;

.section/pm seg_pmco;

_initSPORT:

//============================================================

     //

// Make sure that the multichannel mode registers are cleared

//

//============================================================

r0 = 0;

dm(SPMCTL0) = r0;

dm(SPMCTL1) = r0;

dm(SPMCTL2) = r0;

dm(SPCTL0) = r0;

dm(SPCTL1) = r0;

dm(SPCTL2) = r0;

//============================================================

//

// Configure SPORT 0 as a receiver (input from ADC)

//

//    OPMODE = I2S mode

//    SLEN24 = 24 bit of data in each 32-bit word

//    SPEN_A = Enable data channel A

//

//------------------------------------------------------------

r0 = OPMODE | SLEN24 | SPEN_A;

dm(SPCTL0) = r0;

//============================================================

//

// Configure SPORTs 1 & 2 as transmitter (output to DACs 1-4)

//

//    SPTRAN = Transmit on serial port

//    OPMODE = I2S mode

//    SLEN24 = 24 bit of data in each 32-bit word

//    SPEN_A = Enable data channel A

//    SPEN_B = Enable data channel B

//

//------------------------------------------------------------

r0 = SPTRAN | OPMODE | SLEN24 |SPEN_B ;

dm(SPCTL1) = r0;

dm(SPCTL2) = r0;

r14=0xFFFFFFFF;

r15=0xFFFFFFFF;

r3=22;      //initialize  shift of float conversion

r5=0;       //adaptation modes

r1=HCountInit;

dm(HCount)=r1;

b0=Mike;

l0=MikeTaps;

m0=1;

b8=H;

l8=HTaps;

m8=1;

r1=HTaps;

f5=0;

r9=0;       //initial mode

rts;

_initSPORT.end: 

Parents
  •      Hello,

         The latency is not from the SHARC or its programming, but from the on-board AD1835 Codec.  The EZ-Kit board relies on this chip to get analog audio in and out.  Generally these codecs have built-in decimation and interpolating filters to avoid aliasing at the ADC and reconstruct the output at the DAC.  Their combined group delay adds up neatly to the 1.3 mS latency you observed:

         Best regards,

         Bob

Reply
  •      Hello,

         The latency is not from the SHARC or its programming, but from the on-board AD1835 Codec.  The EZ-Kit board relies on this chip to get analog audio in and out.  Generally these codecs have built-in decimation and interpolating filters to avoid aliasing at the ADC and reconstruct the output at the DAC.  Their combined group delay adds up neatly to the 1.3 mS latency you observed:

         Best regards,

         Bob

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.