Post Go back to editing

Problems with ADSP21262 JTAG interface and Building

My configurations are: Visual DSP++ 5.0, ADSP-21262SBBC-150 and ADZS-HPUSB-ICE.

The target board design has been confirmed with ADSP21262 EZ-KIT-Lite design reference and the appendix A in EE-68.

Question 1: Confirming with EE-175, ICE TEST was successful, but the JTAG frequency selection ‘Test’ couldn’t pass ‘Memory verification’.

Why?

Question 2: the CLK_CFG1:CLK_CFG0=1:0, which means CCLK:CLKIN = 8:1. When CLKIN is 10MHz or 13.3MHz, there are both ERROR

(0x80048008): Opcode scan: Do scan error.

JTAG scan failed-Check target power and emulator connection

DSP could not generate emulator interrupt

Why does this happen?

Question 3: BUT the target could be connected when CLKIN is 40MHz or 20MHz (also CCLK:CLKIN = 8:1)!

Why?

Question 4: Connect the target with 40MHz or 20MHz CLKIN(CCLK:CLKIN = 8:1), When I build any File, it’s OK. But when building the Project, there is always

‘Failed to set automatic breakpoint at ‘main’ ’!

Even building the ADSP21262 example in Visual DSP++ 5.0, there is the same error!

Why does this happen?

Please help me!

Thanks very much!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.