programming PCG for SPDIF clock

Hello,

I want to set internal adsp 21364 clock as a clock for sampling in SPDIF, using the SPDIF talkthru, I've programmed PCG correctly, but I recieve crackles with output audio signal. The code with comments is below.

#define CLKA_DIVIDER 8 //--provides SCLK serial clock to S/PDIF TX and SPORT0

#define FSA_DIVIDER 512//--provides Frame Sync to S/PDIF TX and SPORT0 (approx 48kHz)

#define CLKB_DIVIDER 2 //--provides HFCLK to S/PDIF TX

{

  *pPCG_CTLA_1 = CLKA_DIVIDER;

  *pPCG_CTLA_0 = FSA_DIVIDER | ENFSA | ENCLKA ;

  *pPCG_CTLB_1 = CLKB_DIVIDER | 0xC00000;

  *pPCG_CTLB_0 = ENCLKB ;

  *pPCG_PW = 0;

  *pPCG_SYNC = 0;

}

Sru :

void InitDAI(){

// Disable the pull-up resistors on all 20 pins

    *pDAI_PIN_PULLUP = 0x000FFFFF;

//  Tie the pin buffer input LOW.

    SRU(LOW,DAI_PB18_I);

//  Tie the pin buffer enable input LOW

    SRU(LOW,PBEN18_I);

    SRU(DAI_PB18_O,DIR_I);

    //  Clock in from SPDIF RX

    SRU(PCG_CLKA_O,SPORT0_CLK_I);//DIR_CLK_O

    //  Frame sync from SPDIF RX

    SRU(DIR_FS_O,SPORT0_FS_I);//DIR_FS_O //when i change this FS into PCG fs i recieve just crackles, but very loud

    //  Data in from SPDIF RX

    SRU(DIR_DAT_O,SPORT0_DA_I);

    // Clock on pin 7

    SRU(PCG_CLKA_O,DAI_PB07_I);//DIR_CLK_O

    SRU(HIGH,PBEN04_I);

    SRU(PCG_CLKB_O,DAI_PB04_I);//TUTAJ SPRAWDZAMY ZEGARY

    SRU(HIGH,PBEN17_I);

   

    // Frame sync on pin 8

    SRU(PCG_FSA_O,DAI_PB08_I);//DIR_FS_O

    // Data in on pin 5

    SRU(DAI_PB05_O , SPORT0_DB_I);

    // Tie the pin buffer enable inputs HIGH to drive DAI pins 7 and 8

    SRU(HIGH,PBEN07_I );

    SRU(HIGH,PBEN08_I );

//-----------------------------------------------------------------------------

//

//  Connect the DACs: The codec accepts a BCLK input from DAI pin 13 and

//          a LRCLK (a.k.a. frame sync) from DAI pin 14 and has four

//          serial data outputs to DAI pins 12, 11, 10 and 9

//

//          Connect DAC1 to SPORT1, using data output A

//          Connect DAC2 to SPORT1, using data output B

//          Connect DAC3 to SPORT2, using data output A

//          Connect DAC4 to SPORT2, using data output B

//

//          Connect MCLK from SPDIF to DAC on DAI Pin 6

//

//          Connect the clock and frame sync inputs to SPORT1 and SPORT2

//          should come from the SPDIF RX on DAI pins 7 and 8, respectively

//

//          Connect the SPDIF RX BCLK and LRCLK out to the DAC on DAI

//          pins 13 and 14, respectively.

//

//          All six DAC connections are always outputs from the SHARC

//          so tie the pin buffer enable inputs all high.

//

//------------------------------------------------------------------------

//  Connect the pin buffers to the SPORT data lines

    SRU(SPORT2_DB_O,DAI_PB09_I);

    SRU(SPORT2_DA_O,DAI_PB10_I);

    SRU(SPORT1_DB_O,DAI_PB11_I);

    SRU(SPORT1_DA_O,DAI_PB12_I);

//------------------------------------------------------------------------

//  Connect the clock, frame sync, and MCLK from the SPDIF RX directly

//    to the output pins driving the DACs.

    SRU(PCG_CLKA_O,DAI_PB13_I);//DIR_CLK_O

    SRU(PCG_FSA_O,DAI_PB14_I);//DIR_FS_O

    SRU(PCG_CLKB_O,DAI_PB06_I);//DIR_TDMCLK_O

//------------------------------------------------------------------------

//  Connect the SPORT clocks and frame syncs to the clock and

//    frame sync from the SPDIF receiver

    SRU(PCG_CLKA_O,SPORT1_CLK_I);//DIR_CLK_O

    SRU(PCG_CLKA_O,SPORT2_CLK_I);//DIR_CLK_O

    SRU(PCG_FSA_O,SPORT1_FS_I);//DIR_FS_O

    SRU(PCG_FSA_O,SPORT2_FS_I);//DIR_FS_O

//------------------------------------------------------------------------

//  Tie the pin buffer enable inputs HIGH to make DAI pins 6 & 9-14 outputs.

    SRU(HIGH,PBEN06_I);

    SRU(HIGH,PBEN09_I);

    SRU(HIGH,PBEN10_I);

    SRU(HIGH,PBEN11_I);

    SRU(HIGH,PBEN12_I);

    SRU(HIGH,PBEN13_I);

    SRU(HIGH,PBEN14_I);

}

can anybody tell what am i doing wrong? I just want to have SPDIF signal clocked by the internal clock, not the one recovered from SPDIF signal...

Parents Reply Children
No Data