Post Go back to editing

Reading ADSP-21261 Processor with minimal components

Thread Summary

The user asked if it's possible to read the ADSP-21261 SHARC processor ID via JTAG without the SPI flash and 25 MHz crystal installed. The final answer confirmed that a power supply and clock source are required for JTAG communication, and the 25 MHz crystal or an external clock must be connected. Additional advice was given to ensure no input pins are left floating to avoid functional issues.
AI Generated Content

Hi

Is it possible to read a SHARC processor ID WITHOUT the SPI flash installed, via the ICE tool ? I developed a custom board and doing basic tests like power and processor communication,  the only components populated are X2 4.7k pull-up resistors (FOR THE JTAG LINE ), is it possible to read the processor with minimal amount of components ?

The processor is a ADSP-21261. (also the 25.00MHZ oscillator crystal is NOT connected), So far I cannot communicate with the processor at all.

I need this to verify that the power supply and processor is working.

Parents
  • Hi,

    Yes, even without a SPI Flash device you should be able to connect to the processor via JTAG . But for this to work , you have to make sure that the power, JTAG circuitry is correct (refer to the ADSP-21261 EzKit Schematic) and a proper Clock input source. Also the processor input pins should not be left floating(CLKCFGx, BOOTCFGx, CLKIN etc )Generally the datasheet pin description will have this information. Once you get these basic things right, you should be able to connect the processor through JTAG with the help of ICE

    Regards,

    Mahesh

Reply
  • Hi,

    Yes, even without a SPI Flash device you should be able to connect to the processor via JTAG . But for this to work , you have to make sure that the power, JTAG circuitry is correct (refer to the ADSP-21261 EzKit Schematic) and a proper Clock input source. Also the processor input pins should not be left floating(CLKCFGx, BOOTCFGx, CLKIN etc )Generally the datasheet pin description will have this information. Once you get these basic things right, you should be able to connect the processor through JTAG with the help of ICE

    Regards,

    Mahesh

Children
No Data