Post Go back to editing

intermittent booting please help

Can someone please help me Im really stuck

I built a ADSP-21261 custom board, the system seems to have successfully booted via from M2516 SPI flash (in master mode), however im finding a problem with intermittent booting,where the board doesn't successfully boot the system first time during power up, most of the time I have to power cycle the board quite a few times to get the board to boot correctly.

Note: the program is very simple it just toggles Flag1 so no PLL software setup was used and the clock config is set to 3:1, this is obviously used to test the the boot sequence.

I've read all most of the SHARCEE engineering docs referenced on the forum, so far I haven't found a solution or cause to why this is happening the docs does have alot of useful information which I have taken into consideration, but this problem seems unique.

This experiences seems similar to post https://ez.analog.com/message/138620#138620 however im using a ADSP-21261

Here is my setup

1) I'm using CCES 1.0.3

2) Here is my cldp command (which seems to work)

cldp -proc ADSP-21262 -emu "ICE-100" -driver "C:\Users\admin\CrossCore Embedded Studio\examples\21262_ezkit_lite_1.0.0\M25P16_Flasher\Debug\M2516_Flasher.dxe"   -cmd prog -erase all -format hex -file "C:\Users\admin\CrossCore Embedded Studio\examples\21262_ezkit_lite_1.0.0\Core_Timer\Debug\Core_Timer.ldr"  -cmd compare  -format hex  -offset 0  -file "C:\Users\admin\CrossCore Embedded Studio\examples\21262_ezkit_lite_1.0.0\Core_Timer\Debug\Core_Timer.ldr"

3) See attachment for my SHARC loader settings.

4) I'm using the default kernel, I'm using the following CrossCore Embedded Studio 1.0.3\SHARC\ldr\26x_spi.dxe

5) Find some attachments illustrating the problem

attachments.zip
Parents
  • I'm not sure if this is an issue, I doubt it is see attachment.

    The ADSP-21262 (200Mhz) shows a example external crystal of 12.5Mhz with PLL multiplier of 16:1 thats 12.5 x 16 = 200MHz during boot,

    However, Im using a ADSP-21261 (150Mhz) with a 25MHz crystal with a PLL multiplier of 3:1 thats 25 * 3 = 75Mhz during boot.

    My question is will the lowered clock rate of 75MHz cause an issue during SPI boot?Can this be responsible for the intermittent booting I'm experiencing?

Reply
  • I'm not sure if this is an issue, I doubt it is see attachment.

    The ADSP-21262 (200Mhz) shows a example external crystal of 12.5Mhz with PLL multiplier of 16:1 thats 12.5 x 16 = 200MHz during boot,

    However, Im using a ADSP-21261 (150Mhz) with a 25MHz crystal with a PLL multiplier of 3:1 thats 25 * 3 = 75Mhz during boot.

    My question is will the lowered clock rate of 75MHz cause an issue during SPI boot?Can this be responsible for the intermittent booting I'm experiencing?

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.