Post Go back to editing

how can i write/read two bytes to the TWI interface using ADSP21489?

Hi  everyone

                I ues the TWI interface of SHARC reading the tempereture sensor.Now, i use the example of the Power_On_Self_Test  and  i can write/read one byte data to the TWI interface. But i can not  write/read two bytes to the TWI interface.

              MY slave is the tmp112,i read the datasheet, the time diagram is below.

   

//THE CODE        

void I2C_Master_Write (unsigned int data, unsigned int address)
{

/* setup flag */
g_write_pend = 1;

/* write address to the 8-bit TX fifo */
*pTXTWI8 = address;

/* enable master transfer complete and TX FIFO service interrupts */
*pTWIIMASK = TWIMCOM | TWITXINT;

/* setup for 2 data bytes, master enable, master TX */
*pTWIMCTL = TWIDCNT2 | TWIMEN;

/* wait for data */
while ( g_buff_empty != 1 )
{
;
}

/* write data to the 8-bit TX fifo */
*pTXTWI8 = data;

/* reset flag */
g_buff_empty = 1;

/* wait for write to complete */
while( g_write_pend == 1 )
{
;
}

/* write data to the 8-bit TX fifo */
*pTXTWI8 = data;

/* reset flag */
g_buff_empty = 1;

/* wait for write to complete */
while( g_write_pend == 1 )
{
;
}

}


int Read_TWI_Register(int address)
{
int temp; /* temporary int */


/* setup flags, to read we do both write and read */
g_write_pend = 1;
g_read_pend = 1;

/* write address to the 8-bit TX fifo */
*pTXTWI8 = address;

/* enable master transfer complete interrupt */
*pTWIIMASK = TWIMCOM;

/* setup for 1 data byte, master enable, master TX */
*pTWIMCTL = TWIDCNT1 | TWIMEN;

/* wait for write to complete */
while( g_write_pend == 1 )
{
;
}

/* setup for 1 data byte, master enable, master RX */
*pTWIMCTL = TWIDCNT1 | TWIMEN | TWIMDIR;

/* wait for read to complete */
while( g_read_pend == 1 )
{
;
}

/* read data from the 8-bit RX fifo */
temp = *pRXTWI8;

return temp;
}

catching  the wave from the OSC

the write

the read

hope someone can give me some advice,thanks.

                                                                              jack

attachments.zip
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.