SHARC boot sequence. Help needed.

Hi,

Maybe someone could help me with boot kernel information I miss.

I try to fix a device where the ADSP-21266SKSTZ-1B. The processor was getting hot, it was impossible to connect with HP-USB debug probe so first of all I've replaced it.

After such action the IC doesn't get hot anymore, debug connection seems possible.

It looks lile the processor loads 256 words of boot kernel, because after connecting the debug probe end generating reset the core stops at address 80005 (which seems to be the boot kernel entry point).

After starting the code, it goes to a loop, and seem to stuck at following instructions

[0008001D] r1=pass r1;
[0008001E] if eq jump (pc, 0xffffffff);

I can tell that the boot kernel was read from flash correctly via parallel port, because the first 256 words at address 0x00080000 (internal SRAM) match the words at address 0x01000000 (external Flash).

The processor has the BOOT_CFG lines configured for Parallel Port Boot via EPROM boot.

Looks like the communication via parallel bus works fine (boot kernel in Flash/ 1M x 8bit accessible, external SRAM/ 128k x *bit at 0x01400000 also seems to work fine / is writable, preserves data).

I've attached the boot kernel dump (from RAM) as disassembly.

I suspect that the code for mentioned loop waits for the SPI or Parallel Port interrupt, but I'm not sure what rationale for that would it have at boot stage here.

At the stage when execution stucks at the mentioned loop, in the LIRPTL following flags are set:

ppiM, spilM.

Is that possile that the SHARC processor waits for the another processor (which it's interconnected with SPI interface) to be given boot info for regions to be loaded into the internal RAM?

That assumption appeared when I took a look at the original 26x_prom.asm boot kernel assembly.

I'll add any more information you need (about the hardware and content of the registers of processor when debugging the code) if necessary.

Any help would be greatly appreciated.

boot_kernel.asm.zip
  • 0
    •  Analog Employees 
    on Nov 15, 2016 7:41 AM

    If you are using a modified boot kernel, try using the default boot kernel supplied with VisualDSP++ together with a simple example application (LED blink or Flag Toggle) to confirm basic boot-loading.

     

    Please look into the below FAQ to debug the target which fails to boot.

    FAQ: How to debug a target board which boots from Flash? 

  • Hi Jithul,

    Thank zou for your reply.

    I'm currently unable to write the flash memory. What I confirmed is, that the boot kernel code in RAM at boot match first 256 words of external Parallel Flash at address 0x01400000.

    The code starts executing, but it stops at loop.

    What I need help in, is determining what the loop wait for.

    At the stage, it looks like the PPI and SPI interrupts are enabled.

    Can you help what is the purpose of the loop below?

    r1=pass r1;

    if eq jump (pc, 0xffffffff);

    Full boot kernel code attached.

    Thanks.

  • 0
    •  Analog Employees 
    on Nov 18, 2016 5:29 AM

    Hello,

    Please see my suggestion given below to find the root cause of booting issue.

    • Were you able to successfully boot your ADSP-21266 custom board ever before?
    • Ensure that the /TRST signal of the JTAG ICE is connected to board ground. Do not leave this signal floating. Letting this signal float may cause boot failures or other memory access failures.
    • Ensure that you have selected the correct parameters while generating the .LDR file. Selecting an inappropriate parameter may cause the boot to fail (please share the screenshot of your configuration)
    • Ensure that the correct boot kernel is used before generating the loader (.LDR) file. If you are using a modified boot kernel, try using the default boot kernel supplied with VisualDSP++ together with an example application to confirm basic boot-loading.
    • Verify the Power-Up Sequencing timing diagram which is mentioned in the ADSP-21266 datasheet(Page no:17). Make sure that  the processor is properly coming out of RESET.
    • Make sure that the PLL is configured correctly. The default boot kernel may have the PLL configuration as per the EZ-KIT Lite board. This need to be changed if your application uses a different CLKIN. Check the CLKCFG signals and ensure that the PLL is not overdriven. Ensure that the ratio selected in combination with the CLKIN frequency does not exceed the core clock to a value greater than specified.

     

    Regards,

    Jithul

  • As I said this is a device I have little knowledge about. I try to fix it.

    What I do have is boot kernel assembler dump and a schematics.

    The primary question is why it waits in the loop I mentioned about. I know a lot about ARM assembler, but not much about SHARC.

    Anyone coud explain what may be the meaning of following loop, and direct me what to check to get to know about what goes wrong, so that the boot sequence freeze?

    [0008001D] r1=pass r1;
    [0008001E] if eq jump (pc, 0xffffffff);

    Is the r1 supposed to be modified by interrupt handler code?

  • 0
    •  Analog Employees 
    on Nov 24, 2016 6:40 AM

    Can you please load the dxe of kernel file to view its debug Symbols, you will need to choose 'File'->'Load Symbols', and select your kernel DXE file. This will help you to understand where exactly processor stuck in the Kernel file.