Post Go back to editing

Inquiry on DAI I/O port of ADSP-21483.

Hello.

This is an inquiry on DAI I/O port of ADSP-21483.

Are these I2S in, I2S output and SPDIF I/O port simultaneously working?

As per Serial Ports (SPORTs) in page 9 of datasheet,

One SPORT provides two transmit signals while the other SPORT provides the two receive signals.

 

And there is no description on DAI_01 ~ DAI_18 in page.61 Lead Name.  I need information on port assignment.