Post Go back to editing

SigmaStudio + ADSP SC-589:  First startup - please help

Hello everyone - 1 noob here.  Trying to fire up the EZ-Kit / SC-589 for the first time.  I seem to encounter some glitches that the manual (http://www.analog.com/media/en/dsp-documentation/evaluation-kit-manuals/adsp-sc589-ezboard-manual.pdf ) does not stipulate.

I have CCES 2.5.0, SigmaStudio 3.14, as well SigmaStudio for SHARC / SHARC AudioToolbox.

My board is hooked up, ICE-1000 + kit-SD-card inserted. 

*  But my USB in the HardwareConfig window is 'red'

*  CompilerOutput says DXE not loaded for SHARC

*  There are 2 yellow LEDs flashing under the IDE-connection points, as well three yellow LEDs on the opposite side of the board

If anyone could give me a brief super-quick intro to fire this thing up it would be very appreciated indeed.  Thank you all in advance!

Parents
  • Hi there,

    I have installed the below packages:

    I have tried to load the DXEs from this location initially, but they don't seem to work:

    There are several dxe-files on my system, but I do not know which one to use:

    It is all a bit confusing at the moment, but in parallel here I am in the processing of debugging / initializing the EZ-board with help from support, so I am hoping that will bring me one step closer to making the board accessible / programmable directly from SigmaStudio

    :-)

    Cheers!

Reply
  • Hi there,

    I have installed the below packages:

    I have tried to load the DXEs from this location initially, but they don't seem to work:

    There are several dxe-files on my system, but I do not know which one to use:

    It is all a bit confusing at the moment, but in parallel here I am in the processing of debugging / initializing the EZ-board with help from support, so I am hoping that will bring me one step closer to making the board accessible / programmable directly from SigmaStudio

    :-)

    Cheers!

Children
No Data