Hi all,
I can't find any information on the signal delay that the SPDIF receiver and transmitter introduce.
I assume that the transmitter does not generate signal latency at all, however the receiver should.
So, let's assume the following:
DSP 1 generates a master clock, outputs a signal via ADCs and passes this signal via SPDIF transmitter to DSP2
DSP2 uses the recovered clocks and outputs the received signal via ADC.
Currently, I measure a delay of 3.5 samples at 48 kHz between these 2 analog signals.
But there should be any official information about this, shouldn't it?
Best regards,
Rainer
Hi Jithul,
well, the lower the better. I have to deal with this latency to get the two DSPs in sync and just want to know if this is the lowest I can get.
Also, I wanted to have an official number for it to be sure to do everything right.
Best regards,
Rainer
Hi Jithul,
well, the lower the better. I have to deal with this latency to get the two DSPs in sync and just want to know if this is the lowest I can get.
Also, I wanted to have an official number for it to be sure to do everything right.
Best regards,
Rainer