Hi all,
I can't find any information on the signal delay that the SPDIF receiver and transmitter introduce.
I assume that the transmitter does not generate signal latency at all, however the receiver should.
So, let's assume the following:
DSP 1 generates a master clock, outputs a signal via ADCs and passes this signal via SPDIF transmitter to DSP2
DSP2 uses the recovered clocks and outputs the received signal via ADC.
Currently, I measure a delay of 3.5 samples at 48 kHz between these 2 analog signals.
But there should be any official information about this, shouldn't it?
Best regards,
Rainer
Hi again,
since there are no responses from AD and I needed some answers, I measured a system with SPDIF receiver and transmitter directly connected at 48 and 96 kHz, finding that the latency introduced by this system is 3.5 samples.
If somebody has alternative facts, just let me know.
Regards,
Rainer
Hi again,
since there are no responses from AD and I needed some answers, I measured a system with SPDIF receiver and transmitter directly connected at 48 and 96 kHz, finding that the latency introduced by this system is 3.5 samples.
If somebody has alternative facts, just let me know.
Regards,
Rainer