Hello, I want to use AD1933 as slave, it connect with ADSP21489. In ADSP21489, I use PCGA generate CLK(3.072M) and frame sync clock(48k) to AD1933. And I send a sinusoidal signal, but the AD1933 output pin have not ideal output, it is discontinuous, look at the piecture 1. But I changed AD1933 as master and ADSP21489 as slave, the ad1933 output is pure sinusoidal signal.
I don't know what 's happened.
I pushed my code pieces, someone help me to look what wrong, thanks.
situation for ADSP21489 slave, AD1933 Master:
unsigned char ConfigParam1939 [] = { (AD1939_ADDR), DACMUTE, 0x00, (AD1939_ADDR), CLKCTRL0, DIS_ADC_DAC | INPUT256 | PLL_IN_MCLK | MCLK_OUT_OFF | PLL_PWR_DWN, (AD1939_ADDR), CLKCTRL1, DAC_CLK_PLL | ADC_CLK_PLL | DIS_VREF, //////1 #ifdef USE_48_KHZ_SAMPLE_RATE (AD1939_ADDR), DACCTRL0, DAC_FMT_I2S | DAC_BCLK_DLY_1 | DAC_SR_48K,#endif#ifdef USE_96_KHZ_SAMPLE_RATE (AD1939_ADDR), DACCTRL0, DAC_FMT_I2S | DAC_BCLK_DLY_1 | DAC_SR_96K,#endif#ifdef USE_192_KHZ_SAMPLE_RATE (AD1939_ADDR), DACCTRL0, DAC_FMT_I2S | DAC_BCLK_DLY_1 | DAC_SR_192K,#endif (AD1939_ADDR), DACCTRL1, DAC_BCLK_MASTER| DAC_LRCLK_MASTER| DAC_CHANNELS_2 | DAC_LATCH_MID | DAC_BCLK_SRC_PIN, //2 (AD1939_ADDR), DACCTRL1, DAC_BCLK_MASTER| DAC_LRCLK_MASTER | DAC_CHANNELS_2 | DAC_LATCH_MID | DAC_BCLK_SRC_PIN, //Ddebug (AD1939_ADDR), DACCTRL2, DAC_WIDTH_24 ,
//(AD1939_ADDR), AUXCTRL0, AUX_LATCH_MID | AUX_FMT_I2S | AUX_BCLK_DLY_1 | AUX_WIDTH_24, //(AD1939_ADDR), AUXCTRL1, AUX_BCLK_SRC_PIN | AUX_CHANNELS_2 | AUX_LRCLK_FMT_50_50|AUX_LRCLK_POL_NORM|AUX_BCLK_POL_NORM, // NDdebug (AD1939_ADDR), DACVOL_L1, DACVOL_MAX, (AD1939_ADDR), DACVOL_R1, DACVOL_MAX, (AD1939_ADDR), DACVOL_L2, DACVOL_MAX, (AD1939_ADDR), DACVOL_R2, DACVOL_MAX, (AD1939_ADDR), DACVOL_L3, DACVOL_MAX, (AD1939_ADDR), DACVOL_R3, DACVOL_MAX, (AD1939_ADDR), DACVOL_L4, DACVOL_MAX, (AD1939_ADDR), DACVOL_R4, DACVOL_MAX, (AD1939_ADDR), CLKCTRL0, DIS_ADC_DAC | PLL_IN_MCLK | MCLK_OUT_XTAL | INPUT256 | PLL_PWR_UP, (AD1939_ADDR), CLKCTRL0, ENA_ADC_DAC | PLL_IN_MCLK | MCLK_OUT_XTAL | INPUT256 | PLL_PWR_UP, (AD1939_ADDR), DACMUTE, 0x00, } ;
Above config AD1939, it works fine.
And I change it to slave, just change a little like this, note that the red area.
.....
AD1939_ADDR), DACCTRL1, DAC_BCLK_SLAVE| DAC_LRCLK_SLAVE| DAC_CHANNELS_2 | DAC_LATCH_MID | DAC_BCLK_SRC_PIN, //2 (AD1939_ADDR), DACCTRL1, DAC_BCLK_SLAVE| DAC_LRCLK_SLAVE | DAC_CHANNELS_2 | DAC_LATCH_MID | DAC_BCLK_SRC_PIN, //Ddebug
and code piece in DSP:
int reg=0,r0,i; int fs_div = MCLK/RATE_SAMPLES; int sclk_div = MCLK/(RATE_SAMPLES*32*2);
* pPCG_CTLA1 =0 ; *pPCG_CTLA0 =0; for(i=0;i<10000;i++);//delay //*pPCG_PW = 32*2; r0 = sclk_div | CLKASOURCE | FSASOURCE | ((sclk_div/2)<<20) ; *pPCG_CTLA1 = r0 ; r0 = fs_div ; *pPCG_CTLA0 = r0; r0 = ENFSA | ENCLKA ; *pPCG_CTLA0 |= r0;
config PCGA , it worked. But the ad1933 output is not normal.
So I want to know if I config AD1933 as slave mode correct?
if right, it it must be pcg clock is wrong, how to do it?
Also I have a question about phase shift, I don't know why there is ((sclk_div/2)<<20), I just do it as looking at datasheet. if someone explain it to me , I am very appreciative!
Hello,
Sorry for the delay in response on this. Are you still working on this issue?
I have attached an example code for ADSP-21479 processor where AD1939 configured as slave. Here the PCG is configured to generate Master clock, Bit clock and Frame Sync. In the coded we used PCGs which have an option to synchronize the frame sync output using the external trigger.
Please note that when you have set the ADC into AUX mode it changes the way the pins are used. Look at the Table 11. Pin Function Changes in TDM-AUX Mode in AD1933 datasheet. Please check if this causes the issue in getting no signal. Can you please change the configuration from AUX to TDM and see if the problem is still persist.
Best Regards,
Jithul