Post Go back to editing

ADSP-21469 not booting after being programmed

I programmed my ADSP-21469 EzKit successfully using the CLDP and an ICE-1000. I set the loader file up to program the parallel flash memory. The command line reported that the programming was done. I set the boot switch (sw4) to position 2 for booting from the parallel flash memory. Then I reset my board.

Unfortunately it seems that either the program didn't take, or the board isn't booting. I'm not sure what the problem is but the program runs fine when I run it though CCES and the emulator, but I just can't seem to get it to run on it's own. Any help you can give me would be much appreciated.

Parents
  • Please see my comments.

    1) I don't think you are not using correct diver file for parallel flash.  Looking at the image showed above, seems the driver file is for SPI flash (M25P16).

    Please use the driver file for parallel flash (M29W320) from the below path,

    <ADSP-21469 BSP installation directory>\ADSP-21469_EZKIT-Rel1.0.0\21469_EZ-Board\Examples\Device_Programmer\parallel\21469_m29w320_dpia.dxe

    2) Please confirm if you have modified the driver file that you used above. Just wondering how it shows the DevCode, ManCode and all stuffs?

    Best Regards,

    Jithul

     

Reply
  • Please see my comments.

    1) I don't think you are not using correct diver file for parallel flash.  Looking at the image showed above, seems the driver file is for SPI flash (M25P16).

    Please use the driver file for parallel flash (M29W320) from the below path,

    <ADSP-21469 BSP installation directory>\ADSP-21469_EZKIT-Rel1.0.0\21469_EZ-Board\Examples\Device_Programmer\parallel\21469_m29w320_dpia.dxe

    2) Please confirm if you have modified the driver file that you used above. Just wondering how it shows the DevCode, ManCode and all stuffs?

    Best Regards,

    Jithul

     

Children
No Data