Post Go back to editing

ADSP-21469 not booting after being programmed

I programmed my ADSP-21469 EzKit successfully using the CLDP and an ICE-1000. I set the loader file up to program the parallel flash memory. The command line reported that the programming was done. I set the boot switch (sw4) to position 2 for booting from the parallel flash memory. Then I reset my board.

Unfortunately it seems that either the program didn't take, or the board isn't booting. I'm not sure what the problem is but the program runs fine when I run it though CCES and the emulator, but I just can't seem to get it to run on it's own. Any help you can give me would be much appreciated.

Parents
  • I loaded the file that you sent me onto the ADSP-21469. I had to modify the script txt slightly by pointing it to the driver dxe I have here, and to use the ICE-1000.

    Everything seems to have gone okay with the deployment.

    I hit the reset button on the board but the LED turned on and stayed green. Should it be flashing on and off if it booted the program here?

Reply
  • I loaded the file that you sent me onto the ADSP-21469. I had to modify the script txt slightly by pointing it to the driver dxe I have here, and to use the ICE-1000.

    Everything seems to have gone okay with the deployment.

    I hit the reset button on the board but the LED turned on and stayed green. Should it be flashing on and off if it booted the program here?

Children
No Data