Post Go back to editing

Porting software  from ADSP-21489 to ADSP-21573 and ADSP-SC573 

Customer ask some questions.

Right now we have  plenty of software for ADSP-21489, but it’s quite hard to port it to ADSP-SC573 family. Code itself

is 99% C and C++.

 

Does family ADSP-SC573 have interface with external static memory like AMI for ADSP-21489? If not than how can we ensure

interaction with external static memory (RD, WE, CS, A, D)?

 

We have about 3-6 ADSP-21489 processors on the board. One of them is loading initializer program from

Flash memory, that is reading programs for other processors from Flash memory and loads them through

SPI-slave mode. After loading of satellites main processor is reloaded from the same Flash memory but already by

working program.

Can we organize a similar scheme with ADSP-SC573 board as master processor and ADSP-21573 as slave?

 

What if ADSP-21573 will be both master and slave?

 

Since processor has 2 or 3 cores more than one programmer will be working on software development. How is

ROM code merged(code polling)? Each core has its own loaded file or each time all codes are compiling? Is

there possibility to watch this process “ live”?

 

Now we need to store several programs for one processor in ROM. When system starts one of the

processors loads (in future - ARM core) and upon analysis of system configuration several additional

processors are loaded  (in future - SHARC ADSP-SC573 core) from different ROM addresses. In this case how

can we organize loading of different programs for SHARC cores with the same program for ARM core?

Parents
  • Customer have another question:

    The main target of the external parallel interface is connection FPGA and nvSRAM to store the event log (not distorted when power is off). How can these connections be formed? Working through a parallel port requires too much development effort.

    It seems that  in the description of the processor  is a description of the SMC.

    As I understood , SMC is a static memory controller.  is that the thing we need?

Reply
  • Customer have another question:

    The main target of the external parallel interface is connection FPGA and nvSRAM to store the event log (not distorted when power is off). How can these connections be formed? Working through a parallel port requires too much development effort.

    It seems that  in the description of the processor  is a description of the SMC.

    As I understood , SMC is a static memory controller.  is that the thing we need?

Children
No Data