Post Go back to editing

SPORT primary and secondary on EV-SOMCRR-EZLITE

Thread Summary

The user asked how to configure the ADSP-21569 SOM with the EV-SOMCRR-EZLITE to receive all 4 channels from the ADAU1372 via DMA. The solution involves using the ADI_SPORT_CHANNEL_PRIM_SEC configuration, which interleaves the channels as CH1 | CH3 | CH2 | CH4.
AI Generated Content
Category: Software
Product Number: ADSP-21569
Software Version: CCES 2.12.1

Hey together, 

we have the ADSP-21569 SOM with the EV-SOMCRR-EZLITE and we want to understand the SPORT handling more in detail. So far we are able to run the example code for the ADAU1372 and receive and transmit 2 channels from and to the mini jacks. We are also able to switch the configuration from slave to master and so on. 

As the ADAU1372 offers 4 channels in total which are provided as 2x 2CH I2S stream we want to receive all 4 channels via DMA in the ADSP. 

ADAU1372 LRCLK <- DAI_PIN01 <- SPORT3A LRCLK

ADAU1372 BCLK <- DAI_PIN02 <- SPORT3A BCLK

ADAU1372 DAC DATA <- DAI_PIN03 <- SPORT3A DATA_D0

ADAU1372 ADC DATA 0 -> DAI_PIN04 -> SPORT3B DATA_D0

ADAU1372 ADC DATA 1 -> DAI_PIN05 -> SPORT3B DATA_D1

Depending on the configuration we can receive either channel 1&2 or channel 3&4. This works perfectly fine. We provided 2 compile options here to switch. 

Compile to receive channel 1&2: 

eResult = adi_sport_DMATransfer(hSPORTDev3BRx,&iSRC_LIST_1_SP3B,(DMA_NUM_DESC),ADI_PDMA_DESCRIPTOR_LIST, ADI_SPORT_CHANNEL_PRIM);

Compile to receive channel 3&4 

eResult = adi_sport_DMATransfer(hSPORTDev3BRx,&iSRC_LIST_3_SP3B,(DMA_NUM_DESC),ADI_PDMA_DESCRIPTOR_LIST, ADI_SPORT_CHANNEL_SEC);

But what to we have to do to receive all 4 channels? If we call both functions, even with different descriptors, we dont receive anything. Then we thought about the option ADI_SPORT_CHANNEL_PRIM_SEC, this seems not to work. What do we have to do to receive via both data lines SDATA_D0 and SDATA_D1 in one half SPORT? 

The examples es checked always use different half SPORTs or only one dataline. 

Best regards,

Eric 

Thread Notes