We are developing a AMP product with ADSP21565. According to the system design, the input source of 21565 is A2B TDM16, and the output sink signal is TDM8. So, we need to use PCG to do 2-division the input clock so that the output clock could be synchronized with that of the inputs. The main SRU connections are defined as below:
-----------------------------------------------------------------------------------------------------------------------------------------------------------------
//DAI0_PB03_I is as the input BCK clock from A2B
DAI1_CRS_PB03_O --> PCG0_EXTCLKD_I //external clock source of PCG comes in by crossing through DAI0 to DAI1
PCG0_CLKD_O --> DAI1_PB06_I //PCG BCK clock out
PCG0_FSD_O --> DAI1_PB05_I //PCG FS clock out
DAI0_PB04_O --> DAI0_PB04_I //input FS clock
//DAI0_PB04_I is as the input FS clock from A2B
DAI1_CRS_PB04_O --> SPT4A_FS_I //external FS coming by crossing through DAI0 to DAI1 is directly as the FS clock source of SPORT4A
DAI1_CRS_PB03_O --> SPT4A_CLK_I //external BCK coming by crossing through DAI0 to DAI1 is directly as the BCK clock source of SPORT4A
SPT4A_D0_O --> DAI1_PB08_I //DAI1_PB08_O is as the data output of SPORT4A
PCG0_CLKD_O --> SPT4B_CLK_I // BCK clock from PCG is as the BCK clock source of SPORT4B
PCG0_FSD_O --> SPT4B_FS_I // FS clock from PCG is as the FS clock source of SPORT4B
SPT4B_D0_O --> DAI1_PB09_I //DAI1_PB09_O is as the data output of SPORT4B
------------------------------------------------------------------------------------------------------------------------------------------------------------------------
The PCG configuration is as picture below:

With the SRU configuration above, we can see data pumped out from SPORT4A (which is clocked by external clock pair of BCK & FS), but we failed to catch any data pumped out from SPORT4B (which is clocked by PCG outputs). The input BCK & FS we caught is as picture below:

The BCK & FS coming out of PCG was caught as picture below:

As we can see above, the differences between SPORT4A and SPORT4B are as below:
1. SPORT4A is with TDM16, while SPORT4B is with TDM8;
2. SPORT4A is clocked by the input clock pair directly; while SPORT4B is clocked by the PCG clock outputs.
I don't think TDM16 or TDM8 configuration could cause the fail of SPORT4B as long as the configuration of SPORT4B could match the sequence of its clock inputs(BCK & FS out of PCG).
Could you tell me why we can not drive the SPORT data out by PCG clock?
Thank you!
Edit Notes
modify a typo: DAI0_PB04_O --> DAI0_PB04_I //input BCK clock ==>DAI0_PB04_O --> DAI0_PB04_I //input FS clock[edited by: humorhxu at 5:19 AM (GMT -4) on 28 Oct 2024]