Post Go back to editing

The data that appears in SPORT is different from the internal data.

Category: Software
Product Number: ADSP-21489
Software Version: CCES2.11

The signal is sent to SPORT by DMA.
When the digital signal is locked or unlocked, the normal sine wave may be distorted.
In this case, the internal value and the external value through SPORT by DMA may be different, resulting in distortion.
The reason for the difference is that there are 4 output channels, 2 channels are not distorted, 2 channels are distorted, and the internal values are the same for all 4 channels. 2 channels have the same data output from the DSP and 2 channels have different data output.
This phenomenon will continue to occur even if the lock is unlocked/locked unless the DSP is reset.
How is it possible that the internal data and the data coming out of the DMA are different?
How can I fix this?
This is occurring with the ADSP-21489, but does it not occur with the ADSP-21565?


Parents Reply Children
  • Hi.

    This question has come up.

      I am using DMA to move files.
      Do I have to stop the next DMA until the file has been moved?

    1:The signal flow looks like this.

    The problem is that the actual value input to D/ACONVERTER is different from the value of FILE MOVE-2 in DSP.

    2:SET_SPORT3:
    b7=STP3a_cp;
    r15=STP3a_ii; r14=0xFFFFF; r15=r15 and r14; dm(i7,1)=r15; // Chainning Next Set Address Chaining
    r15=data_W; dm(i7,1)=r15; // Internal Number of words
    r15=1; dm(i7,1)=r15; // Internal Address Increment
    r15=tx3a_C; dm(i7,1)=r15; // Internal Starting Address Index
    b7=STP3b_cp;
    r15=STP3b_ii; r14=0xFFFFF; r15=r15 and r14; dm(i7,1)=r15; // Chainning Next Set Address Chaining
    r15=data_W; dm(i7,1)=r15; // Internal Number of words
    r15=1; dm(i7,1)=r15; // Internal Address Increment
    r15=tx3b_D; dm(i7,1)=r15; // Internal Starting Address Index
    rts;
    GO_SPORT3:
    r15=0; dm(SPCTL3)=r15; // disable Serial PORT3 DMA
    ustat1 = OPMODE| //I2S mode enable ('1')
    SPTRAN| //Transmit on enabled channels
    SLEN32| //32-bit word length
    /// L_FIRST| //I2S transmit left channel first ('1') 
    SPEN_A| //Enable Channel A
    SDEN_A| //Enable Channel A DMA
    SCHEN_A| //Enable Channel A DMA Chaining
    SPEN_B| //Enable Channel B
    SDEN_B| //Enable Channel B DMA
    SCHEN_B; //Enable Channel B DMA Chaining
    dm(SPCTL3)=ustat1; // Enable Serial PORT3 DMA Start
    r15=STP3a_ii; dm(CPSP3A)=r15;
    r15=STP3b_ii; dm(CPSP3B)=r15;
    // bit set IMASK SP3I; //SPORT3 Interrupt Mask
    rts;

    3:All are the same from 44k to 192k.

    4:No errors or exceptions

    Thanks & Best Regards,

    YAMAMOTO

  • Hi Yamato,

    The location of the DMA parameters for the next sequence comes from the chain pointer register that points to the next set of DMA parameters

    stored in the processor’s internal memory. In chained DMA operations, the processor automatically initializes and then begins another DMA transfer when the current DMA transfer is complete.

    Could you please share us the DAC part and its configurations.

    Regards,
    Divya.P

  • Hi.

    I believe this is not a DAC problem, but a DMA problem.
    As you can see in the picture, the top two waveforms are distorted.
    However, the data inside the DSP is the same for all four.
    The data sent out by the DMA does not match the internal data.
    I have not been able to solve the problem because I do not know why this is happening.
    Question.
    Is it possible to send DMA 3 and 5 in sequence without using a chain?



    Thanks, & Best Regards,

    YAMAMOTO

  • Hi Yamamato,
     

    For further analysis, Could you please share the simple project that replicates the issue.

    Regards,
    Divya.P

  • Hi.

    'Could you please share the simple project that replicates the issue.'

    What should I do?

    What should I tell you?
     Programs?

    Thanks & Best regards,

    YAMAMOTO

  • Hi Yamamoto,

    Our sincere apologies for the delay.

    Please find the attached code, which is configured with SPORT 1 as receiver and SPORT 3&5 as transmitter with 4 channels provided as input in chained DMA. We have tested this in 21469 Ez-kit. Please modify this and try this code in your end and let me know the results.
    1.AD1939_I2S_Sampled_Based_Talkthru_Sport3_5.zip
    Regards,
    Divya.P