Post Go back to editing

SPORT Interrupt not triggered

Category: Software
Product Number: ADSP-21569

Hello,

I'm using a 24.576 MHz MCLK input on Pin DAI0_04, which is routed to PCG A to generate the clocks for TDM8. The whole clock routing is working properly (checked with scope).

My DAC is connected to SPORT 2A and is working as it should (checked with the output of testdata and ) So DMA and SPORT config must be correct.

The ADC is connected to SPORT 4A, the MCU input to SPORT 7A. The settings are identical (despite the direction of data transfer). The clocks from PCG A are routed to DAI pins via CRS. From the output pins I routed to the SPORTS clk and fs inputs. The clock signals show up on the pins as expected.

The problem is: both registered SPORT callbacks (SPORT 2A and 7A) are not triggered (the counter "SPORT_CB_counter" is checked in the main loop and a print is output every 1000 cycles).

Am I missing something? Please have a short look at the code.

Kind regards,
Markus

//======= PCG Init =======

//Includes
#include <services/pcg/adi_pcg.h>
#include "Driver_PCG.h"
#include "Driver_Debug.h"


//Functions
void PCG_Init(void){

	//BCLK config TDM8
	ADI_PCG_CLK_INFO PCG_CLK_Inf_TDM8 =
	{
		ADI_PCG_CLK_EXT,              	//Clock Source
		2u,          					//Clock Divisor for 12.288 MHz
		false                           //External Trigger
	};

	//FS config for 48 kHz, TDM8
	ADI_PCG_FS_INFO PCG_FS_Inf_TDM8 =
	{
		ADI_PCG_FS_EXT,                	//Clock Source
		512u,     					   	//Frame Sync Divisor 48 KHz
		256u,                           //Pulse Width
		1u,                             //Phase shift for edge sync = clk_div / 2
		false,                         	//External Trigger
		ADI_PCG_FSBYPASS_MODE_NORMAL   	//Bypass Mode normal
	};

	//Init
	adi_pcg_Init(ADI_PCG_DEV_A, &PCG_CLK_Inf_TDM8, &PCG_FS_Inf_TDM8);
}


//======= SPU Init =======
//Includes
#include <stdint.h>
#include <stdio.h>
#include <services/spu/adi_spu.h>
#include "Driver_SPU.h"
#include "Driver_SPORT.h"
#include "Driver_Debug.h"

//SPU IDs, p.
#define UART0_SPU_PID       29
#define UART0_Rx_DMA_SPU    65
#define UART0_Tx_DMA_SPU    66

#define SPORT_0A_SPU  		13
#define SPORT_0B_SPU  		14
#define SPORT_1A_SPU  		15
#define SPORT_1B_SPU  		16
#define SPORT_2A_SPU  		17
#define SPORT_2B_SPU  		18
#define SPORT_3A_SPU  		19
#define SPORT_3B_SPU  		20
#define SPORT_4A_SPU  		21
#define SPORT_4B_SPU   		22
#define SPORT_5A_SPU  		23
#define SPORT_5B_SPU   		24
#define SPORT_6A_SPU  		25
#define SPORT_6B_SPU   		26
#define SPORT_7A_SPU  		27
#define SPORT_7B_SPU   		28

#define SPORT_0A_DMA_SPU  	49
#define SPORT_0B_DMA_SPU  	50
#define SPORT_1A_DMA_SPU  	51
#define SPORT_1B_DMA_SPU  	52
#define SPORT_2A_DMA_SPU  	53
#define SPORT_2B_DMA_SPU  	54
#define SPORT_3A_DMA_SPU  	55
#define SPORT_3B_DMA_SPU  	56
#define SPORT_4A_DMA_SPU  	57
#define SPORT_4B_DMA_SPU   	58
#define SPORT_5A_DMA_SPU  	59
#define SPORT_5B_DMA_SPU   	60
#define SPORT_6A_DMA_SPU  	61
#define SPORT_6B_DMA_SPU   	62
#define SPORT_7A_DMA_SPU  	63
#define SPORT_7B_DMA_SPU   	64

//Variables
static uint8_t SpuMemory[ADI_SPU_MEMORY_SIZE];

static ADI_SPU_HANDLE hSpu;			//SPU handle

//SPORT - Make SPORTs to generate secure transactions
//ADC
eResult = adi_spu_EnableMasterSecure(hSpu, SPORT_4A_SPU, true);
if(eResult != ADI_SPU_SUCCESS){
	printf("Error: SPU Secure Transfer not possible! Errorcode: 0x%08X\n", eResult);
}
eResult = adi_spu_EnableMasterSecure(hSpu, SPORT_4A_DMA_SPU, true);
if(eResult != ADI_SPU_SUCCESS){
	printf("Error: SPU Secure Transfer not possible! Errorcode: 0x%08X\n", eResult);
}

//MCU
eResult = adi_spu_EnableMasterSecure(hSpu, SPORT_7A_SPU, true);
if(eResult != ADI_SPU_SUCCESS){
	printf("Error: SPU Secure Transfer not possible! Errorcode: 0x%08X\n", eResult);
}
eResult = adi_spu_EnableMasterSecure(hSpu, SPORT_7A_DMA_SPU, true);
if(eResult != ADI_SPU_SUCCESS){
	printf("Error: SPU Secure Transfer not possible! Errorcode: 0x%08X\n", eResult);
}

//DAC
eResult = adi_spu_EnableMasterSecure(hSpu, SPORT_2A_SPU, true);
if(eResult != ADI_SPU_SUCCESS){
	printf("Error: SPU Secure Transfer not possible! Errorcode: 0x%08X\n", eResult);
}
eResult = adi_spu_EnableMasterSecure(hSpu, SPORT_2A_DMA_SPU, true);
if(eResult != ADI_SPU_SUCCESS){
	printf("Error: SPU Secure Transfer not possible! Errorcode: 0x%08X\n", eResult);
}
	
	
	
	
//======= SRU Init =======

//Port Input Enable Control Register
*pREG_PADS0_DAI0_IE = BITM_PADS_DAI0_IE_VALUE;
*pREG_PADS0_DAI1_IE = BITM_PADS_DAI1_IE_VALUE;


//---- MCLK Input ----
SRU(LOW, DAI0_PBEN04_I);			//Set pinbuf to input
SRU(DAI0_PB04_O, PCG0_EXTCLKA_I);	//Route clock input to PCG A
SRU(DAI0_PB04_O, PCG0_EXTCLKB_I);	//Route clock input to PCG B

//Route PCG A fs as trigger source to PCG B
//SRU(PCG0_FSA_O, PCG0_SYNC_CLKB_I);


//---- Clocks ----
//DAC - SPORT2A
SRU(HIGH, DAI0_PBEN03_I);			//Output
SRU(PCG0_CLKA_O, DAI0_PB03_I);		//PCG A clk to DAC MCLK pin

SRU(HIGH, DAI0_PBEN06_I);			//Output
SRU(PCG0_CLKA_O, DAI0_PB06_I);		//PCG A clk to DAC BCLK pin
SRU(PCG0_CLKA_O, SPT2_ACLK_I);		//PCG A clk to SPORT 2A

SRU(HIGH, DAI0_PBEN02_I);			//Output
SRU(PCG0_FSA_O, DAI0_PB02_I);		//PCG A fs to DAC LRCLK pin
SRU(PCG0_FSA_O, SPT2_AFS_I);		//PCG A clk to SPORT 2A


//MCU - SPORT7A (CRS)
SRU2(HIGH, DAI1_PBEN04_I);			//Output
SRU2(PCG0_CRS_CLKA_O, DAI1_PB04_I);	//PCG A clk to MCU MCLK pin (CRS)

SRU2(HIGH, DAI1_PBEN02_I);			//Output
SRU2(PCG0_CRS_CLKA_O, DAI1_PB02_I);	//PCG A clk to MCU BCLK pin (CRS)
SRU2(DAI1_PB02_O, SPT7_ACLK_I);		//PCG A clk to SPORT 7A

SRU2(HIGH, DAI1_PBEN01_I);			//Output
SRU2(PCG0_CRS_FSA_O, DAI1_PB01_I);	//PCG A fs to MCU LRCLK pin (CRS)
SRU2(DAI1_PB01_O, SPT7_AFS_I);		//PCG A fs to SPORT 7A


//ADC - SPORT4A
SRU(HIGH, DAI0_PBEN12_I);			//Output
SRU(PCG0_CLKA_O, DAI0_PB12_I);		//PCG A clk to ADC MCLK pin

SRU(HIGH, DAI0_PBEN20_I);			//Output
SRU(PCG0_CLKA_O, DAI0_PB20_I);		//PCG A clk to ADC BCLK pin
SRU2(DAI1_PB02_O, SPT4_ACLK_I);		//PCG A clk from MCU BCLK pin to SPORT 4A

SRU(HIGH, DAI0_PBEN19_I);			//Output
SRU(PCG0_FSA_O, DAI0_PB19_I);		//PCG A fs to ADC LRCLK pin
SRU2(DAI1_PB01_O, SPT4_AFS_I);		//PCG A fs from MCU LRCLK pin to SPORT 4A


//---- Data pins ----
//ADC
SRU2(LOW, DAI1_PBEN19_I);			//Input
SRU2(DAI1_PB19_O, SPT4_AD0_I); 		//SPORT 4A

//MCU
SRU2(LOW, DAI1_PBEN03_I);			//Input
SRU2(DAI1_PB03_O, SPT7_AD0_I); 		//SPORT 7A

//DAC
SRU(HIGH, DAI0_PBEN01_I);			//Output
SRU(SPT2_AD0_O, DAI0_PB01_I); 		//SPORT 2A





//======= Driver SPORT =======

//Includes
#include <stdint.h>
#include <stdio.h>
#include <string.h>
#include <services/int/adi_int.h>
#include <drivers/sport/adi_sport.h>
#include "Driver_SPORT.h"
#include "Driver_DMA.h"
#include "Driver_Debug.h"
#include <math.h>

//Definitions

//Variables
//Memory required for SPORTs
static uint8_t SPORTMemory0A[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory0B[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory1A[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory1B[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory2A[ADI_SPORT_MEMORY_SIZE];

static uint8_t SPORTMemory4A[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory5A[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory5B[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory6A[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory7A[ADI_SPORT_MEMORY_SIZE];

//SPORT Handles
static ADI_SPORT_HANDLE hSPORT_0A     	= NULL;
static ADI_SPORT_HANDLE hSPORT_0B     	= NULL;
static ADI_SPORT_HANDLE hSPORT_1A     	= NULL;
static ADI_SPORT_HANDLE hSPORT_1B 	  	= NULL;
static ADI_SPORT_HANDLE hSPORT_2A_DAC 	= NULL;		//DAC

static ADI_SPORT_HANDLE hSPORT_4A_ADC 	= NULL;		//ADC in
static ADI_SPORT_HANDLE hSPORT_5A_DANTE	= NULL;		//DANTE in
static ADI_SPORT_HANDLE hSPORT_5B     	= NULL;
static ADI_SPORT_HANDLE hSPORT_6A_AES 	= NULL;		//AES in
static ADI_SPORT_HANDLE hSPORT_7A_MCU 	= NULL;		//MCU in

static volatile bool block_number = 0;

ADI_CACHE_ALIGN int32_t DAC_Buffer1[BLOCKSIZE * TDM8_NB_CH] = {};
ADI_CACHE_ALIGN int32_t DAC_Buffer2[BLOCKSIZE * TDM8_NB_CH] = {};

ADI_CACHE_ALIGN int32_t ADC_Buffer1[BLOCKSIZE * TDM8_NB_CH] = {};
ADI_CACHE_ALIGN int32_t ADC_Buffer2[BLOCKSIZE * TDM8_NB_CH] = {};

ADI_CACHE_ALIGN int32_t MCU_Buffer1[BLOCKSIZE * TDM8_NB_CH] = {};
ADI_CACHE_ALIGN int32_t MCU_Buffer2[BLOCKSIZE * TDM8_NB_CH] = {};


//Function prototypes
void SPORT4A_ADC_Cb(void *pAppHandle, uint32_t nEvent, void *pArg);
void SPORT2A_DAC_Cb(void *pAppHandle, uint32_t nEvent, void *pArg);
void SPORT7A_MCU_Cb(void *pAppHandle, uint32_t nEvent, void *pArg);

void FillDACBufferWithTestdata(void);

//Function definitions
void SPORT_Init(void){

    ADI_SPORT_RESULT eResult;

    //FillDACBufferWithTestdata();

	//---- SPORT Device 4A - ADC ----
	eResult = adi_sport_Open(4u, ADI_HALF_SPORT_A, ADI_SPORT_DIR_RX, ADI_SPORT_MC_MODE, SPORTMemory4A, ADI_SPORT_MEMORY_SIZE, &hSPORT_4A_ADC);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config data: datatype zero fill, word length 32 bit, MSB first, DMA packing disabled, right-justified disabled
	eResult = adi_sport_ConfigData(hSPORT_4A_ADC, ADI_SPORT_DTYPE_ZERO_FILL, 31u, false, false, false);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config clock: internal clock ratio (ignored), use external clock, sample data on rising edge, disable gated clock
	eResult = adi_sport_ConfigClock(hSPORT_4A_ADC, 0u, false, false, false);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config fs: slot width 32 bit, fs required, use external fs, data-independent fs (ignored in MC mode), active low fs, early fs, edge sensitive fs
	eResult = adi_sport_ConfigFrameSync(hSPORT_4A_ADC, 31u, true, false, true, false, false, true);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config MC: fs delay 1 bclk, 8 slots, window start 0, mc dma data packing disabled
	eResult = adi_sport_ConfigMC(hSPORT_4A_ADC, 1u, 7u, 0u, false);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config channels: starting ch nb 0, end ch nb 7
	eResult = adi_sport_SelectChannel(hSPORT_4A_ADC, 0u, 7u);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}
	DEBUG_PRINT("SPORT 4A opened and configured\n");

	//Register SPORT Callback function
	eResult = adi_sport_RegisterCallback(hSPORT_4A_ADC, SPORT4A_ADC_Cb, NULL);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}
	DEBUG_PRINT("SPORT 4A cb registered\n");


	//---- SPORT Device 2A - DAC ----
	eResult = adi_sport_Open(2u, ADI_HALF_SPORT_A, ADI_SPORT_DIR_TX, ADI_SPORT_MC_MODE, SPORTMemory2A, ADI_SPORT_MEMORY_SIZE, &hSPORT_2A_DAC);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config data: datatype zero fill, word length 32 bit, MSB first, DMA packing disabled, right-justified disabled
	eResult = adi_sport_ConfigData(hSPORT_2A_DAC, ADI_SPORT_DTYPE_ZERO_FILL, 31u, false, false, false);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config clock: internal clock ratio (ignored), use external clock, sample data on rising edge, disable gated clock
	eResult = adi_sport_ConfigClock(hSPORT_2A_DAC, 0u, false, false, false);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config fs: slot width 32 bit, fs required, use external fs, data-independent fs (ignored in MC mode), active low fs, early fs, edge sensitive fs
	eResult = adi_sport_ConfigFrameSync(hSPORT_2A_DAC, 31u, true, false, true, false, false, true);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config MC: fs delay 1 bclk, 8 slots, window start 0, mc dma data packing disabled
	eResult = adi_sport_ConfigMC(hSPORT_2A_DAC, 1u, 7u, 0u, false);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config channels: starting ch nb 0, end ch nb 7
	eResult = adi_sport_SelectChannel(hSPORT_2A_DAC, 0u, 7u);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}
	DEBUG_PRINT("SPORT 2A opened and configured\n");


	//---- SPORT Device 7A - MCU ----
	eResult = adi_sport_Open(7u, ADI_HALF_SPORT_A, ADI_SPORT_DIR_RX, ADI_SPORT_MC_MODE, SPORTMemory7A, ADI_SPORT_MEMORY_SIZE, &hSPORT_7A_MCU);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config data: datatype zero fill, word length 32 bit, MSB first, DMA packing disabled, right-justified disabled
	eResult = adi_sport_ConfigData(hSPORT_7A_MCU, ADI_SPORT_DTYPE_ZERO_FILL, 31u, false, false, false);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config clock: internal clock ratio (ignored), use external clock, sample data on rising edge, disable gated clock
	eResult = adi_sport_ConfigClock(hSPORT_7A_MCU, 0u, false, false, false);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config fs: slot width 32 bit, fs required, use external fs, data-independent fs (ignored in MC mode), active low fs, early fs, edge sensitive fs
	eResult = adi_sport_ConfigFrameSync(hSPORT_7A_MCU, 31u, true, false, true, false, false, true);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config MC: fs delay 1 bclk, 8 slots, window start 0, mc dma data packing disabled
	eResult = adi_sport_ConfigMC(hSPORT_7A_MCU, 1u, 7u, 0u, false);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	//Config channels: starting ch nb 0, end ch nb 7
	eResult = adi_sport_SelectChannel(hSPORT_7A_MCU, 0u, 7u);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}
	DEBUG_PRINT("SPORT 7A opened and configured\n");

	//Register SPORT Callback function
	eResult = adi_sport_RegisterCallback(hSPORT_7A_MCU, SPORT7A_MCU_Cb, NULL);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}
	DEBUG_PRINT("SPORT 7A cb registered\n");


	//Init peripheral DMA descriptors
	PDMA_Init();


	//---- Init first DMA transfer ----
	eResult = adi_sport_DMATransfer(hSPORT_4A_ADC, &DMA_Desc_ADC_1, DMA_NUM_DESC, ADI_PDMA_DESCRIPTOR_LIST, ADI_SPORT_CHANNEL_PRIM);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	eResult = adi_sport_DMATransfer(hSPORT_2A_DAC, &DMA_Desc_DAC_1, DMA_NUM_DESC, ADI_PDMA_DESCRIPTOR_LIST, ADI_SPORT_CHANNEL_PRIM);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}

	eResult = adi_sport_DMATransfer(hSPORT_7A_MCU, &DMA_Desc_MCU_1, DMA_NUM_DESC, ADI_PDMA_DESCRIPTOR_LIST, ADI_SPORT_CHANNEL_PRIM);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT Error! Errorcode: 0x%08X\n", eResult);}
	DEBUG_PRINT("SPORT DMA started\n");


	//---- Enable data transfer ----
	eResult = adi_sport_Enable(hSPORT_4A_ADC, true);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT 4A Error! Errorcode: 0x%08X\n", eResult);}

	eResult = adi_sport_Enable(hSPORT_2A_DAC, true);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT 2A Error! Errorcode: 0x%08X\n", eResult);}

	eResult = adi_sport_Enable(hSPORT_7A_MCU, true);
	if(eResult != ADI_SPORT_SUCCESS) {DEBUG_PRINT("SPORT 7A Error! Errorcode: 0x%08X\n", eResult);}


	DEBUG_PRINT("SPORTs enabled\n");
}

volatile uint32_t SPORT_CB_counter = 0;

void SPORT7A_MCU_Cb(void *pAppHandle, uint32_t nEvent, void *pArg){

	SPORT_CB_counter++;
	uint8_t offset = 0;

	switch (nEvent){
		case ADI_SPORT_HW_ERR_PRIMARY_CHNL_OVERFLOW:	//Rx mode
			break;
		case ADI_SPORT_HW_ERR_FS:
			break;
		case ADI_SPORT_HW_ERR_DMA:
			break;

		case ADI_SPORT_EVENT_RX_BUFFER_PROCESSED:
			//Copy ADC buf to DAC buf
			if(block_number == 0){
				//memcpy(DAC_Buffer1, ADC_Buffer1, (BLOCKSIZE * TDM8_NB_CH * 4));

				for(uint16_t i=0; i < (BLOCKSIZE * TDM8_NB_CH); i+=8)
				{
					DAC_Buffer1[i]   = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+1] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+2] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+3] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+4] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+5] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+6] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+7] = ADC_Buffer1[i+offset];
				}
			}
			else{
				//memcpy(DAC_Buffer2, ADC_Buffer2, (BLOCKSIZE * TDM8_NB_CH * 4));

				for(uint16_t i=0; i < (BLOCKSIZE * TDM8_NB_CH); i+=8)
				{
					DAC_Buffer2[i]   = ADC_Buffer2[i];
					DAC_Buffer2[i+1] = ADC_Buffer2[i];
					DAC_Buffer2[i+2] = ADC_Buffer2[i];
					DAC_Buffer2[i+3] = ADC_Buffer2[i];
					DAC_Buffer2[i+4] = ADC_Buffer2[i];
					DAC_Buffer2[i+5] = ADC_Buffer2[i];
					DAC_Buffer2[i+6] = ADC_Buffer2[i];
					DAC_Buffer2[i+7] = ADC_Buffer2[i];
				}
			}
			block_number = !block_number;

			break;

		default:
	    	break;
	}
}

void SPORT4A_ADC_Cb(void *pAppHandle, uint32_t nEvent, void *pArg){

	SPORT_CB_counter++;
	uint8_t offset = 0;

	switch (nEvent){
		case ADI_SPORT_HW_ERR_PRIMARY_CHNL_OVERFLOW:	//Rx mode
			break;
		case ADI_SPORT_HW_ERR_FS:
			break;
		case ADI_SPORT_HW_ERR_DMA:
			break;

		case ADI_SPORT_EVENT_RX_BUFFER_PROCESSED:
			//Copy ADC buf to DAC buf
			if(block_number == 0){
				//memcpy(DAC_Buffer1, ADC_Buffer1, (BLOCKSIZE * TDM8_NB_CH * 4));

				for(uint16_t i=0; i < (BLOCKSIZE * TDM8_NB_CH); i+=8)
				{
					DAC_Buffer1[i]   = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+1] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+2] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+3] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+4] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+5] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+6] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+7] = ADC_Buffer1[i+offset];
				}
			}
			else{
				//memcpy(DAC_Buffer2, ADC_Buffer2, (BLOCKSIZE * TDM8_NB_CH * 4));

				for(uint16_t i=0; i < (BLOCKSIZE * TDM8_NB_CH); i+=8)
				{
					DAC_Buffer2[i]   = ADC_Buffer2[i];
					DAC_Buffer2[i+1] = ADC_Buffer2[i];
					DAC_Buffer2[i+2] = ADC_Buffer2[i];
					DAC_Buffer2[i+3] = ADC_Buffer2[i];
					DAC_Buffer2[i+4] = ADC_Buffer2[i];
					DAC_Buffer2[i+5] = ADC_Buffer2[i];
					DAC_Buffer2[i+6] = ADC_Buffer2[i];
					DAC_Buffer2[i+7] = ADC_Buffer2[i];
				}
			}
			block_number = !block_number;

			break;

		default:
	    	break;
	}
}

void SPORT2A_DAC_Cb(void *pAppHandle, uint32_t nEvent, void *pArg){

	SPORT_CB_counter++;
	uint8_t offset = 0;

	switch (nEvent){
		case ADI_SPORT_HW_ERR_PRIMARY_CHNL_OVERFLOW:	//Rx mode
			break;
		case ADI_SPORT_HW_ERR_FS:
			break;
		case ADI_SPORT_HW_ERR_DMA:
			break;

		case ADI_SPORT_EVENT_TX_BUFFER_PROCESSED:
			//Copy ADC buf to DAC buf

			if(block_number == 0){
				//memcpy(DAC_Buffer1, ADC_Buffer1, sizeof(DAC_Buffer1));

				for(uint16_t i=0; i < (BLOCKSIZE * TDM8_NB_CH); i+=8)
				{
					DAC_Buffer1[i]   = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+1] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+2] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+3] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+4] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+5] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+6] = ADC_Buffer1[i+offset];
					DAC_Buffer1[i+7] = ADC_Buffer1[i+offset];
				}
			}
			else{
				//memcpy(DAC_Buffer2, ADC_Buffer2, sizeof(DAC_Buffer2));

				for(uint16_t i=0; i < (BLOCKSIZE * TDM8_NB_CH); i+=8)
				{
					DAC_Buffer2[i]   = ADC_Buffer2[i+offset];
					DAC_Buffer2[i+1] = ADC_Buffer2[i+offset];
					DAC_Buffer2[i+2] = ADC_Buffer2[i+offset];
					DAC_Buffer2[i+3] = ADC_Buffer2[i+offset];
					DAC_Buffer2[i+4] = ADC_Buffer2[i+offset];
					DAC_Buffer2[i+5] = ADC_Buffer2[i+offset];
					DAC_Buffer2[i+6] = ADC_Buffer2[i+offset];
					DAC_Buffer2[i+7] = ADC_Buffer2[i+offset];
				}
			}
			block_number = !block_number;

			break;

		default:
	    	break;
	}
}

void FillDACBufferWithTestdata(void){

	double gain_dB = -3;
	double gain = pow(10.0, ((double)gain_dB/20.0));
	bool highorlow = 1;

	for(uint16_t i=0; i < (BLOCKSIZE * TDM8_NB_CH); i+=8)
	{
		if(highorlow){
			DAC_Buffer1[i]   = (int32_t)((double)(0x7FFFFFFF) * gain);
			DAC_Buffer1[i+1] = DAC_Buffer1[i];
			DAC_Buffer1[i+2] = DAC_Buffer1[i];
			DAC_Buffer1[i+3] = DAC_Buffer1[i];
			DAC_Buffer1[i+4] = DAC_Buffer1[i];
			DAC_Buffer1[i+5] = DAC_Buffer1[i];
			DAC_Buffer1[i+6] = DAC_Buffer1[i];
			DAC_Buffer1[i+7] = DAC_Buffer1[i];
		}
		else{
			DAC_Buffer1[i]   = 0;
			DAC_Buffer1[i+1] = 0;
			DAC_Buffer1[i+2] = 0;
			DAC_Buffer1[i+3] = 0;
			DAC_Buffer1[i+4] = 0;
			DAC_Buffer1[i+5] = 0;
			DAC_Buffer1[i+6] = 0;
			DAC_Buffer1[i+7] = 0;
		}
		highorlow = !highorlow;
	}

	memcpy(DAC_Buffer2, DAC_Buffer1, (BLOCKSIZE * TDM8_NB_CH * 4));

	DEBUG_PRINT("DAC buffer filled with testdata\n");
}



//======== DMA Init =========

//Include
#include <stdint.h>
#include <stdio.h>
#include "Driver_DMA.h"
#include "Driver_SPORT.h"
#include "Driver_Debug.h"


//Descriptors
ADI_CACHE_ALIGN ADI_PDMA_DESC_LIST DMA_Desc_ADC_1 = {};
ADI_CACHE_ALIGN ADI_PDMA_DESC_LIST DMA_Desc_ADC_2 = {};

ADI_CACHE_ALIGN ADI_PDMA_DESC_LIST DMA_Desc_DAC_1 = {};
ADI_CACHE_ALIGN ADI_PDMA_DESC_LIST DMA_Desc_DAC_2 = {};

ADI_CACHE_ALIGN ADI_PDMA_DESC_LIST DMA_Desc_MCU_1 = {};
ADI_CACHE_ALIGN ADI_PDMA_DESC_LIST DMA_Desc_MCU_2 = {};



void PDMA_Init(void){

	//2A
	//DAC buffer
	DMA_Desc_DAC_1.pStartAddr	= DAC_Buffer1;
	DMA_Desc_DAC_1.Config		= ENUM_DMA_CFG_XCNT_INT; // | ENUM_DMA_CFG_TRGWAIT;
	DMA_Desc_DAC_1.XCount		= BLOCKSIZE * TDM8_NB_CH;
	DMA_Desc_DAC_1.XModify		= 4;
	DMA_Desc_DAC_1.YCount		= 0;
	DMA_Desc_DAC_1.YModify		= 0;
	DMA_Desc_DAC_1.pNxtDscp		= &DMA_Desc_DAC_2;

	DMA_Desc_DAC_2.pStartAddr	= DAC_Buffer2;
	DMA_Desc_DAC_2.Config		= ENUM_DMA_CFG_XCNT_INT;
	DMA_Desc_DAC_2.XCount		= BLOCKSIZE * TDM8_NB_CH;
	DMA_Desc_DAC_2.XModify		= 4;
	DMA_Desc_DAC_2.YCount		= 0;
	DMA_Desc_DAC_2.YModify		= 0;
	DMA_Desc_DAC_2.pNxtDscp		= &DMA_Desc_DAC_1;

	//4A
	//ADC buffer
	DMA_Desc_ADC_1.pStartAddr	= ADC_Buffer1;
	DMA_Desc_ADC_1.Config		= ENUM_DMA_CFG_XCNT_INT; // | ENUM_DMA_CFG_TRGWAIT;
	DMA_Desc_ADC_1.XCount		= BLOCKSIZE * TDM8_NB_CH;
	DMA_Desc_ADC_1.XModify		= 4;
	DMA_Desc_ADC_1.YCount		= 0;
	DMA_Desc_ADC_1.YModify		= 0;
	DMA_Desc_ADC_1.pNxtDscp		= &DMA_Desc_ADC_2;

	DMA_Desc_ADC_2.pStartAddr	= ADC_Buffer2;
	DMA_Desc_ADC_2.Config		= ENUM_DMA_CFG_XCNT_INT;
	DMA_Desc_ADC_2.XCount		= BLOCKSIZE * TDM8_NB_CH;
	DMA_Desc_ADC_2.XModify		= 4;
	DMA_Desc_ADC_2.YCount		= 0;
	DMA_Desc_ADC_2.YModify		= 0;
	DMA_Desc_ADC_2.pNxtDscp		= &DMA_Desc_ADC_1;

	//7A
	//MCU buffer
	DMA_Desc_MCU_1.pStartAddr	= MCU_Buffer1;
	DMA_Desc_MCU_1.Config		= ENUM_DMA_CFG_XCNT_INT; // | ENUM_DMA_CFG_TRGWAIT;
	DMA_Desc_MCU_1.XCount		= BLOCKSIZE * TDM8_NB_CH;
	DMA_Desc_MCU_1.XModify		= 4;
	DMA_Desc_MCU_1.YCount		= 0;
	DMA_Desc_MCU_1.YModify		= 0;
	DMA_Desc_MCU_1.pNxtDscp		= &DMA_Desc_MCU_2;

	DMA_Desc_MCU_2.pStartAddr	= MCU_Buffer2;
	DMA_Desc_MCU_2.Config		= ENUM_DMA_CFG_XCNT_INT;
	DMA_Desc_MCU_2.XCount		= BLOCKSIZE * TDM8_NB_CH;
	DMA_Desc_MCU_2.XModify		= 4;
	DMA_Desc_MCU_2.YCount		= 0;
	DMA_Desc_MCU_2.YModify		= 0;
	DMA_Desc_MCU_2.pNxtDscp		= &DMA_Desc_MCU_1;
}

  • I did some further testing. I duplicated the settings of PCG A to PCG C. Then I checked if the SPORTs are triggering the interrupt.

    That is working:

    		SRU2(HIGH, DAI1_PBEN01_I);			//Output
    		SRU2(PCG0_FSC_O, DAI1_PB01_I);		//PCG A fs to MCU LRCLK pin
    		SRU2(PCG0_FSC_O, SPT7_AFS_I);		//PCG A fs to SPORT 7A

    Routing the clk signals of a pinbuffer is NOT working:

    		SRU2(HIGH, DAI1_PBEN01_I);			//Output
    		SRU2(PCG0_FSC_O, DAI1_PB01_I);		//PCG A fs to MCU LRCLK pin
    		SRU2(DAI1_PB01_O, SPT7_AFS_I);		//PCG A fs to SPORT 7A

    Could you please explain, why routing directly from the PCG output to the SPORT inputs works and routing the same signal over a pinbuffer and then to the SPORT inputs doesn't work?

    Regards,
    Markus

  • Hi Markus,

    Regarding "Could you please explain, why routing directly from the PCG output to the SPORT inputs works and routing the same signal over a pinbuffer and then to the SPORT inputs doesn't work?"
    >>>Please find the attached code. We tried to replicate your issue using SPORT0A as a transmitter and SPORT0B as a receiver. It's working fine for us.

    Can you please try to probe DAI1_PB01_O? Did you get Framesync.
    ADSP-21569_SPORT.zip
    Regards,
    Divya.P