Post Go back to editing

implementing I2S Input code examples/ demos for Sharc

Product Number: ADZS-21489

I was looking for code examples and demos of I2S implementation but couldn't find any. Can anyone provide me of any help? Thank you.

Parents
  • Hi,

    If you are using CCES, please install the BSP of ADSP-21479 using the link given below:
    download.analog.com/.../ADI_ADSP-21479_EZKIT-Rel1.0.0.exe

    After installation: ..\Analog Devices\ADSP-21479_EZKIT-Rel1.0.0\21479_EZ-Board\Examples\AD1939_I2S_Sample_Based_Talkthru

    Please use this example and change the processor to ADSP-21489 and run it.

    If your using Visual DSP , you can find the I2S sample based talkthrough for 21489 in the below path:
    ..\Program Files (x86)\Analog Devices\VisualDSP 5.1.2\214xx\Examples\ADSP-21489 EZ-Board\21489 AD1939 I2S C Sampled-Based Talkthru

    Regards,
    Divya.P

Reply
  • Hi,

    If you are using CCES, please install the BSP of ADSP-21479 using the link given below:
    download.analog.com/.../ADI_ADSP-21479_EZKIT-Rel1.0.0.exe

    After installation: ..\Analog Devices\ADSP-21479_EZKIT-Rel1.0.0\21479_EZ-Board\Examples\AD1939_I2S_Sample_Based_Talkthru

    Please use this example and change the processor to ADSP-21489 and run it.

    If your using Visual DSP , you can find the I2S sample based talkthrough for 21489 in the below path:
    ..\Program Files (x86)\Analog Devices\VisualDSP 5.1.2\214xx\Examples\ADSP-21489 EZ-Board\21489 AD1939 I2S C Sampled-Based Talkthru

    Regards,
    Divya.P

Children