Post Go back to editing

Triggering multiple dma chains

Category: Choose a category
Product Number: 21489
Software Version: VisualDSP 5.1.2

Hi,

I am trying to implement reads and writes to external memory (SDRAM) via multiple dma chains on a 21489 in assembly. There is an example in the manual but this only explains how to change the direction on the fly and seems to be constantly cycling through the two TCBs.

What I want to do is:

Read two memory blocks from SDRAM => prepare chain of two TCBs

Load first TCB to CECP0

Do something else

poll DMAC0 (look for CHS and DMAS bits)

Do something else

Read two memory blocks from SDRAM => prepare chain of two TCBs

Load first TCB to CECP0

Do something else

poll DMAC0 (look for CHS and DMAS bits)

Do something else

and so on.

My question is, is it enough to configure DMAC0 at the beginning only and the transfers are triggered whenever I write to CPEC0 register?

Or do I have to clear DMAC0 after a chain has finished and reinit it before I start the next chain?

And what is the correct way to poll the DMAC0? Is it right to look for CHS + DMAS? I don't want to go via interrupts.

Raphael

 



fixed some typos
[edited by: rkn at 10:37 PM (GMT -4) on 13 Oct 2022]
Parents Reply Children
No Data