Post Go back to editing

ASM of 21569

Hi,

I write a simple asm code for data copy,but it report a error after running:

A non-recoverable error or exception has occurred.
Description: A parity error has been detected.
General Type: RunTimeError
Specific Type: ParityErrorDetected
Error PC: 0x007fffff

copy.rar

you can see my coed in attachment.

Parents
  • Hi,

    In the code, LCNTR is set as 0. If LCNTR value is zero, the loop will execute to 2^32 times. can you please confirm that you want to execute the loop to 2^32 times.

    We are not able to simulate this issue using "copy.s" file. can you please provide simple project which simulates this issue.

    Regards,
    Anand Selvaraj.

Reply
  • Hi,

    In the code, LCNTR is set as 0. If LCNTR value is zero, the loop will execute to 2^32 times. can you please confirm that you want to execute the loop to 2^32 times.

    We are not able to simulate this issue using "copy.s" file. can you please provide simple project which simulates this issue.

    Regards,
    Anand Selvaraj.

Children
No Data