Post Go back to editing

Uart0 Can't send any character on ADSP-21489 EZ-board

Hi,

   We have a issus about Uart0 on ADSP-21489 EZ-board.

   /*Uart init code*/ 

void initUART(void)

{

/* Sets the Baud rate for UART0 */

*pUART0LCR = UARTDLAB;  //enables access to Divisor register to set bauda rate

*pUART0DLL = 0x8B;      //0x28b = 651 for divisor value and gives a baud rate of 19200 for peripheral clock of 200MHz

    *pUART0DLH = 0x02;

    /* Configures UART0 LCR */

    *pUART0LCR = UARTWLS8; // word length 8

    *pUART0RXCTL = UARTEN;       //enables UART0 in receive mode

    *pUART0TXCTL = UARTEN;       //enables UART0 in core driven mode

}

/*send and receive*/

char getch(void)

{

char ch;

while ((*pUART0LSR & UARTDR) == 0)

{;

}

ch = *pUART0RBR;

return ch;

}

void putch(char ch)

{

while ((*pUART0LSR & UARTTEMT) == 0)

{;

}

*pUART0THR = ch;

}

void putstring(const char *str)

{

char *r = (char *)str-1;

while(*++r){

if(*r == CR) putch(LF);

else if(*r == LF) putch(CR);

putch(*r);

}

return;

}

/*Application code*/

int main( int argc, char *argv[] )

{

   ....

   

initUART();

ch = getch();

putch(ch);

if((ch == 'm') || (ch == 'M')){

sprintf((char *)UARTBuffer,"Uart Init success!! :%f\n", 1.00);

putstring(UARTBuffer);

}

   ....

}

When debug with CCES, we set a breakpoint at line "putstring(UARTBuffer);", If we send a 'm' by PC serials-software, program stop at breakpoint.

and then remove breakpoint, run application get nothing printed on PC serials-software。Why EZ-board can only receive character and nothing

was send.

Parents Reply Children
No Data