Post Go back to editing

Can the ARM core access the DDDR3 memory?

I'm using an ADSP-SC573 with an external DDR3 memory.

I have successfully written a memory test in Core 1 where I write different values from memory position 0x80000000 and forward.

But when I run it in Core 0 (Cortex A5) if hangs when I try to write to the memory. Execution jumps to Data Abort exception handler (adi_rtl_data_abort_hndlr).

Parents
  • Hi,

    By default external memory is divided and accessed as follows:

    Address from 0x80000000 to 0x88FFFFFFu(144MB) for SHARC Cores        
    Address from 0x89000000 to 0x8FFFFFFF(112MB) for ARM core   

    So, you are trying to use the SHARC cores region from ARM core.

    If still you want to use this address region, please follow below steps:
    1. Open Project Arm core > system > linker > apt.c file 2. Change #elif defined(__ADSPSC573__)
        { 0x80000000u, 0x88FFFFFFu, SHARC_L3                    }, /* 144MB DDR-A */
        { 0x89000000u, 0x8FFFFFFFu, ADI_MMU_WB_CACHED           }, /* 112MB DDR-A */
    #endif /* __ADSPSC572__ || __ADSPSC573__ */

     to

    #elif defined(__ADSPSC573__)
        { 0x80000000u, 0x88FFFFFFu, ADI_MMU_RW_UNCACHED         }, /* 144MB DDR-A */
        { 0x89000000u, 0x8FFFFFFFu, ADI_MMU_WB_CACHED           }, /* 112MB DDR-A */
    #endif /* __ADSPSC572__ || __ADSPSC573__ */

    Regards,
    Anand Selvaraj

  • Thank you.

    Then I wonder if it is wrong to test the whole DDR3 memory in Core 1 as following:

    #define DDR_START 0x80000000
    #define DDR_END 0x9FFFFFFF // For my board (4Gb = 536870912 byte)
    //#define DDR_END 0x8FFFFFFF // For ADZS-SC573-EZLITE board (2Gb = 268435456 byte)
    #define STEP 1024
    
    const uint8_t pattern[] = {0xff, 0x55, 0xaa, 0x00};
    uint32_t errors = 0;
    
    printf("START!\n");
    
    for (uint8_t i = 0; i < 4; i++)
    {
      // Fill DDR3 with pattern
      for (uint32_t a = DDR_START; a <= DDR_END; a += STEP)
      {
        *(volatile uint8_t *)a = pattern[i];
      }
    
      // Verify pattern in DDR3
      for (uint32_t a = DDR_START; a <= DDR_END; a += STEP)
      {
        if (*(volatile uint8_t *)a != pattern[i])
        {
          // Found an error
          errors++;
        }
      }
    }
    
    if (errors == 0)
    {
      printf("DDR3 OK\n");
    }
    else
    {
      printf("DDR3 failure\n");
    }

  • Hi,

    You can test the whole DDR3 memory in Core 1. Please refer below example for ddr test:
    <Installation path>\ADSP-SC5xx_EZ-KIT_Lite-Rel2.0.2\ADSP-SC5xx_EZ-KIT\Examples\Power_On_Self_Test\EZ-Board\sc573\sharc

    Regards,
    Anand Selvaraj.

Reply Children
No Data