Hello,
Is there an example of the asynchronous sample rate converter demo available for the ADSP-21479 EZ-Board in CCES?
At the moment I can only find the ASRC demo for 21479 in VisualDSP++.
Thanks and Regards.
Hello,
Is there an example of the asynchronous sample rate converter demo available for the ADSP-21479 EZ-Board in CCES?
At the moment I can only find the ASRC demo for 21479 in VisualDSP++.
Thanks and Regards.
If I were to load the ASRC example for ADSP-21469 onto the ADSP-21479 kit what modifications (if any) would I need to make to the code?
Hi,
Can you please have a look at the example available in the ADSP-21479 Board support package(BSP) to check the DSP. Please download and install the board support package for ADSP-21479 in the below download.analog.com/.../ADI_ADSP-21479_EZKIT-Rel1.0.0.exe
Once you installed, you can find the example code in the below path.
[Installation directory]:\Analog Devices\ADSP-21479_EZKIT-Rel1.0.0\21489_EZ-Board\Examples
Regards,
Anand Selvaraj.
Hi Anand,
Thanks for your reply, the asynchronous sample rate converter example is not available in the ADSP-21479 board support package.
I downloaded the example as part of the ASCR SHARC software module:
There are no CCES examples available for the ADSP-21479.
Regards,
Calum
Hi Anand,
Thanks for your reply, the asynchronous sample rate converter example is not available in the ADSP-21479 board support package.
I downloaded the example as part of the ASCR SHARC software module:
There are no CCES examples available for the ADSP-21479.
Regards,
Calum