Sync PWM0 and PWM1 in ADSP21584

I would like to synchronize the two PWM modules, PWM0 and PWM1, in ADSP21584. The desired behavior is that both PWM modules would run based on their own internal PWMTMR0 respectively and I would like to use TIMER0_TMR0_MST (a trigger master) to synchronize both PWMTMR0 in PWM0 and PWMTMR0 in PWM1.

However, I can't seem to find a trigger slave to synchronize the PWM modules. The TRU has trigger slaves to trip the PWM modules (e.g. PWM0_TRIP_TRIG0), but it does not have trigger slaves to synchronize the PWM modules. 

Am I missing something?

Thanks,

Parents Reply Children