Post Go back to editing

EMAC Example Code Issue

Category: Software
Product Number: ADSP-SC835

I have the  EV-SOMCRR-EZKIT board with ADSP-SC835W and I am trying to test EMAC using the EMAC example code.

While other examples code (like audio talk through ones) worked straigth out of the box, the EMAC examples gives me some error before the Debug even start:

Open On-Chip Debugger (Analog Devices 0.12.0-1.2.0)  OpenOCD 0.12.0 (2025-04-03-09:09)
Licensed under GNU GPL v2
Report bugs to <processor.tools.support@analog.com>
0
Info : only one transport option; autoselecting 'jtag'
adapter speed: 5000 kHz
Info : xtensa permissive mode is disabled
adapter speed: 5000 kHz
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : ADI Debug Agent firmware version is 0.0.9
Info : clock speed 5000 kHz
Info : JTAG tap: adspsc83x.adjc tap/device found: 0x0282c0cb (mfg: 0x065 (Analog Devices), part: 0x282c, ver: 0x0)
Info : JTAG tap: adspsc83x.cpu enabled
Info : [adspsc83x.apb] Examination succeed
Info : [adspsc83x.axi] Examination succeed
Info : [adspsc83x.ahb] Examination succeed
Info : [adspsc83x.sharcfx] Examination succeed
Info : [adspsc83x.m33] Cortex-M33 r1p0 processor detected
Info : [adspsc83x.m33] target has 8 breakpoints, 4 watchpoints
Info : [adspsc83x.m33] Examination succeed
Info : gdb port disabled
Info : gdb port disabled
Info : gdb port disabled
Info : starting gdb server for adspsc83x.sharcfx on 3333
Info : Listening on port 3333 for gdb connections
Info : starting gdb server for adspsc83x.m33 on 3334
Info : Listening on port 3334 for gdb connections
Info : [adspsc83x.sharcfx] Debug controller was reset.
Info : [adspsc83x.sharcfx] Core was reset.
Info : accepting 'gdb' connection on tcp/3333
Info : [adspsc83x.sharcfx] Debug controller was reset.
Info : [adspsc83x.sharcfx] Core was reset.
Info : [adspsc83x.m33] external reset detected
system reset complete
Info : New GDB Connection: 1, Target adspsc83x.sharcfx, state: halted
Error: unable to read from usb to out + buf_index: wanted 24 bytes but only received 0 bytes
Error: return 0
Error: unable to read from usb to out + buf_index: wanted 72 bytes but only received 24 bytes
Error: return 0
Error: Invalid ACK (3) in DAP response
Error: Scan Error!
Error: Invalid ACK (0) in DAP response
Error: Scan Error!
Error: Failed to read memory and, additionally, failed to find out where
Error: unable to read from usb to out + buf_index: wanted 20 bytes but only received 4 bytes
Error: return 0
Error: unable to write from (uint8_t *)&usb_cmd_blk to usb: wanted 12 bytes but only wrote 0 bytes
Error: return -7
Error: Invalid ACK (0) in DAP response
Error: unable to write from (uint8_t *)&usb_cmd_blk to usb: wanted 12 bytes but only wrote 0 bytes
Error: return -7
Error: unable to write from (uint8_t *)&usb_cmd_blk to usb: wanted 12 bytes but only wrote 0 bytes
Error: return -7
Error: unable to write from (uint8_t *)&usb_cmd_blk to usb: wanted 12 bytes but only wrote 0 bytes
Error: return -7
Error: Debug regions are unpowered, an unexpected reset might have happened
Error: JTAG-DP STICKY ERROR
Error: unable to write from (uint8_t *)&usb_cmd_blk to usb: wanted 12 bytes but only wrote 0 bytes
Error: return -7
Error: unable to write from (uint8_t *)&usb_cmd_blk to usb: wanted 12 bytes but only wrote 0 bytes
Error: return -7
Error: Invalid ACK (3) in DAP response
Error: unable to write from (uint8_t *)&usb_cmd_blk to usb: wanted 12 bytes but only wrote 0 bytes
Error: return -7
Error: Debug regions are unpowered, an unexpected reset might have happened
Error: JTAG-DP STICKY ERROR
Error: unable to write from (uint8_t *)&usb_cmd_blk to usb: wanted 12 bytes but only wrote 0 bytes
Error: return -7
Error: Failed to read memory and, additionally, failed to find out where
Error: unable to write from (uint8_t *)&usb_cmd_blk to usb: wanted 12 bytes but only wrote 0 bytes
Error: return -7
Error: Debug regions are unpowered, an unexpected reset might have happened
Error: JTAG-DP STICKY ERROR

I noted that the Debug can actually start if I remove one of these call (no matter wich one):

eMACResult = adi_emac_SubmitDescriptorListRx(hemac,0,emac_desc_rx,NO_OF_DESCS, true); CHECK_EMAC_RESULT(eMACResult);
eMACResult = adi_emac_SubmitDescriptorListTx(hemac,0,emac_desc_tx,NO_OF_DESCS, true); CHECK_EMAC_RESULT(eMACResult);

But if  both TX and RX descriptors submit are present,  the debug is having trouble to load, even if (and I'd like to stress this out) the code never gets to run at all.

Thread Notes

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.