Post Go back to editing

ADSP-2183x/ADSP-SC83x Datasheet errors

Thread Summary

The user reported incorrect polarity for EPWM_CLKSELF (1=FPLL, 0=PCG) on pages 154 and 933 of the ADSP-2183x/ADSP-SC83x SHARC-FX Processor Hardware Reference Manual Rev 0.1, and potential overstrike issues for SPI0_SEL4 and UART1_TX in Table 15 of the ADSP-2183x/ADSP-SC83x Datasheet Rev A. The final answer confirmed the polarity issue and stated that it will be corrected in future updates. The accompanying answer acknowledged the need to check the overstrike issue internally.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADSP-SC835

Hello,

unfortunately the website to submit document errors is broken, so I'll try it here.

ADSP-2183x/ADSP-SC83x SHARC-FX Processor Hardware Reference Manual Rev 0.1:
Page 154 and 933:
EPWM_CLKSELF polarity is wrong, it should be 1=FPLL and 0=PCG. I tested it. In the board support package code it is correct.

ADSP-2183x/ADSP-SC83x Datasheet Rev A:
I didn't test, but I'm pretty sure because there are some inconsistencies: 
Page 33, Table 15 SPI0_SEL4 and UART1_TX -> overstrike missing?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.