Post Go back to editing

XSPI burn

Thread Summary

The user wants to boot from XSPI on the 21835-SOM board using CCES. The solution involves following the 'Creating/Using Loader File' and 'Flashing the Loader file' sections in the 'Readme_Power_On_Self_Test_21835.html', setting the boot mode to 5, and removing the INIT code while creating the loader file. The ADSP-SC83x/ADSP-2183x BSP is required and can be downloaded from the provided link.
AI Generated Content
Category: Software
Product Number: ADSP-2158
Software Version: CCES3.0.2

Hi,

I am using 21835-SOM board and I want to boot from XSPI.So how can I do this via CCES?

Regards,

Bingo

Thread Notes

Parents Reply
  • Hi,

    Can you please follow the "Creating/Using Loader File" and "Flashing the Loader file" section in the "Readme_Power_On_Self_Test_21835.html". Please download and install the ADSP-SC83x/ADSP-2183x BSP from the below link.
    www.analog.com/.../software-download.html

    Once installed, the POST example can be available in the below path.
    [Installation directory]:\Analog Devices\EV-SC8xx_EZ-KIT-Rel1.0.0\EV-SC8xx_EZ-KIT\Examples\Power_On_Self_Test\Power_On_Self_Test_EZ\Readme

    After successfully flashing the loader file, please set the boot mode to 5. Please remove the INIT code while creating the loader file.

    Regards,
    Nandini C

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.