Dear all,
in my software the TWI communication is always distorted, when the processor calculation load on my ADSP-SC835 SHARC-FX DSP gets to high in my audio interrupt service routine of the SPORT audio interface.
I try to change the interrupt priority on a ADSP-SC835 SHARC-FX DSP by using the adi_sec_XXX() functions for the SEC interrupt services. The "migration guide for SHARC+" tells me
"The SEC interrupt service (adi_sec) will also be implemented for SHARC-FX, but is not yet available."
But the adi_sec_XXX() C functions are already available. So I tried to change the interrrupt priority of the TWI interface and the SPORT interface by the following code:
ADI_SEC_RESULT initInterrupts(void)
{
ADI_SEC_RESULT result = adi_sec_SetPriorityLevels(ADI_SEC_CORE_0, ADI_SEC_256_PRIORITY_LEVELS);
if (result)
{
printf("ERROR in adi_sec_SetPriorityLevels: %i\n", result);
return result;
}
int curLevel = 0;
result += adi_sec_SetPriority(INTR_TWI0_DATA, curLevel); curLevel++;
result += adi_sec_SetPriority(INTR_SPORT0_A_DMA, curLevel); curLevel++;
result += adi_sec_SetPriority(INTR_SPORT0_A_STAT, curLevel); curLevel++;
if (result) {
printf("ERROR in adi_sec_SetPriority: %i\n", result);
return result;
}
return ADI_SEC_SUCCESS;
}
But the code doesn't change the interrupt priority at all. The TWI communcation still crashed with to much load in the audio processing interrupt service routine. I see no change, in the behavior. Is the adi_sec really not supported? What do I do wrong?
Best regards
Michael
Ranji - Moved from Other Products (EN) to ADSP-SC83x. Post date updated from Wednesday, March 19, 2025 4:42 PM UTC to Friday, March 21, 2025 11:03 AM UTC to reflect the move.
Hi Michael,
While looking into your query, it seems that the similar query has been handled in private support. Can you please continue the discussion through private support to avoid duplication of efforts.
Regards,
Nandini C