Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
ADSP-SC5xx/ADSP-215xx
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-SC5xx/ADSP-215xx
  • Processors & DSP
  • SHARC Processors
  • ADSP-SC5xx/ADSP-215xx
  • Cancel
ADSP-SC5xx/ADSP-215xx
Documents I want to use the Credit Based Shaping feature to allot a particular bandwidth to Channel 2. How do I program the CBS parameters to achieve the same?
  • Q&A
  • Files
  • Documents
  • Members
  • Tags
  • Cancel
  • +ADSP-SC57x/2157x: FAQ
  • +ADSP-SC58x: FAQ
  • +PMU registers: FAQ
  • +SC58x: FAQ
  • +SHARC+: FAQ
  • +TMU: FAQ
  • +215XX: FAQ
  • +ADC Control Module: FAQ
  • +ADSP-21584: FAQ
  • +ADSP-215xxl: FAQ
  • +ADSP-SC573: FAQ
  • +ADSP-SC5xx/215xx: FAQ
  • +ADSP-SC5xx: FAQ
  • +CCES default startup routine: FAQ
  • +EMAC: FAQ
  • +HADC: FAQ
  • +Hardware Counter based Loops: FAQ
  • +L1 block: FAQ
  • +Preload code customization: FAQ
  • +RDEN bit: FAQ
  • +RGMII/RMII: FAQ
  • +SHARC EE-377: FAQ
  • +Sharc SC584: FAQ
  • +SMMR using MDMA2: FAQ
  • +UCOS: FAQ
  • +USBCLKSEL in CGU_CLKOUT: FAQ
  • ADSP-21569 SPORT single-transmitter multi-receiver example
  • ADSP-SC584 SSL Booting via ROM API from the ARM Cortex A5 (core0), SHARC0 and SHARC1
  • +adsp-sc584: FAQ
  • ADSP-SC594 SPDIF Example
  • ADSP-SC835 SPI Slave transmitter and Master Receiver example code
  • Are code segments placed in block1 and block2, when data caches are enabled?
  • ASRC TDM8/TDM16 Example for ADSP-SC59x
  • Can we use internal pull down resistor for ADSP-SC59x/ADSP-2159x LP_CLK and LP_ACK pins instead of external pull down?
  • +CDU: FAQ
  • Custom Error Handler in Booting for SC594
  • DAI Interrupt example for ADSP-SC573
  • Do ADSP-SC58x/ADSP-SC57x support adi_pkte.h and adi_pka.h?
  • Does QUAD SPI open-drain mode need external pull-up resistors for each of these signals (MISO, MOSI, D2 & D3) in ADSP-21569
  • Does the LRCLK support 50% duty cycle in TDM mode?
  • Does the TMREXP(Timer Expired) pin support in latest SHARC processor?
  • Driver file support for the ADSP-SC584/SC589 custom board, which utilizes the same flash and DDR as Ez-kit.
  • Flash write example for ADSP-SC573 Ez-Kit
  • How many cycles for a cache hit/miss?
  • How many times the DAI can be routed using SRU?
  • How to configure DAI interrupt in ADSP-21569?
  • How to use Assembly to Control Core Flags?
  • How to use PCG trigger event
  • How to use PC_07 instead of SYS_FAULT in ADSP-2156x/ADSP-SC59x/ADSP-2159x ?
  • +IDLE: FAQ
  • Is it possible to change the sampling/driving edges of the ASRC?
  • Is it possible to configure the DSP as Master and Host as Slave once SPI slave booting done?
  • Is it possible to disable/halt/pause the SHARC0/SHARC1 cores from ARM core?
  • Is it possible to verify Secure Booting without programming Keys into OTP Memory?
  • Is the SPIx_RDY signal necessary for SPI slave boot?
  • JEDEC thermal Resistance Data estimation for "θJA, θJC, ΨJT" in ADSP-SC5xx/ADSP-215xx processor.
  • +Local Oscillator: FAQ
  • +MLB channels: FAQ
  • +MSI IDMAC: FAQ
  • Once the processor is locked, is it possible to debug or flash a new application?
  • -Program the CBS parameters: FAQ
    • I want to use the Credit Based Shaping feature to allot a particular bandwidth to Channel 2. How do I program the CBS parameters to achieve the same?
  • +SC57x: FAQ
  • SCB arbitration/priority scheme
  • +Sign and encrypt a normal bootstream: FAQ
  • SPI example for ADSP-SC584
  • SPI secure slave boot
  • +SPORT with ACM: FAQ
  • +SWU: FAQ
  • Understanding Halt feature in ACM Mode
  • Usage of flush_data_buffer api
  • Using MCAPI/MDMA for ADSP-SC594 Dual-SHARC Audio Talkthrough
  • What is "Multiplexed Function Input Tap" available in the "Signal Multiplexing" table in the datasheet.
  • What is the clock configuration (HFCLK, BCLK) required to transmit SPDIF?
  • What is the difference between ENUM_DMA_CFG_XCNT_INT and ENUM_DMA_CFG_PERIPH_INT?
  • What is the recommended TMU_GAIN and TMU_OFFSET value for Calibration?
  • What is the SPORT Latency using DMA between the SHARC cores(Core1 & Core2) for ADSP-SC58x?
  • What is the supported SLCK0 divisor value for ADSP-2156x

I want to use the Credit Based Shaping feature to allot a particular bandwidth to Channel 2. How do I program the CBS parameters to achieve the same?

Consider an example of operating at 100Mbps, and the bandwidth to be allotted to Channel 2 is 60Mbps.

Parameters to be programmed: 1. Send Slope 2. Idle Slope 3. High Credit 4. Low Credit

  • Channel2 idleSlope

  Since bandwidth allocated for Channel 2 is 60%, idleSlope should be 60Mbps.

  Credit accumulation rate = idleSlope = 60 Mbps

  Credit accumulated per cycle (40ns for 100Mbps operation) = 60 Mbps * 40ns = 2.4 bits

  Channel2 idleSlopeCredit Register = 2.4*1024 = 0x99A 

  • Channel2 sendSlope

Since bandwidth allocated for Channel 2 is 60%, sendSlope should be (100-60)Mbps = 40Mbps
  Credit drain rate = sendSlope = 40 Mbps
  Credit drained per cycle (40ns for 100Mbps operation) = 40 Mbps * 40ns = 1.6 bits
  Channel2 sendSlopeCredit Register = 1.6*1024 = 0x666

  • High Credit Value

  This is the maximum value that can be accumulated in the credit parameter, specified in bits scaled by 1,024. The maximum value is maxInterferenceSize, that is, best-effort maximum frame size which is 16,384 bytes or 131,072 bits. The value to be specified is 131,072 * 1,024 = 134,217,728 or 0x0800_0000. 

  • Low Credit Value

This is the minimum value that can be accumulated in the credit parameter, specified in bits scaled by 1,024. The maximum value is maxInterferenceSize, that is, best-effort maximum frame size which is 16,384 bytes or 131,072 bits. The value to be specified is 131,072 * 1,024 = 134,217,728 or 0x0800_0000. The programmed value is 2's complement (negative number), that is, 0xF800_0000.

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • ulizg
    ulizg
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • RE: Happy Computer Security Day! - November 30
    GenevaC
    I have two cybersecurity tips. The first is to verify banking details and email addresses when wiring money, which is crucial. Scammers often exploit slight variations in email addresses or account numbers...
  • RE: AD9371+zc706 transmit and receive signal
    zgy
    The red channel is the rx1 I channel, and the blue channel is the rx2 Q channel. I chose many points to draw the picture because the received data is stable in a short time, but it's amplitude will change...
 
Related Content
  • ulizg
    ulizg
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • RE: Happy Computer Security Day! - November 30
    GenevaC
    I have two cybersecurity tips. The first is to verify banking details and email addresses when wiring money, which is crucial. Scammers often exploit slight variations in email addresses or account numbers...
  • RE: AD9371+zc706 transmit and receive signal
    zgy
    The red channel is the rx1 I channel, and the blue channel is the rx2 Q channel. I chose many points to draw the picture because the received data is stable in a short time, but it's amplitude will change...