Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
ADSP-SC5xx/ADSP-215xx
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-SC5xx/ADSP-215xx
  • Processors & DSP
  • SHARC Processors
  • ADSP-SC5xx/ADSP-215xx
  • Cancel
ADSP-SC5xx/ADSP-215xx
Documents How does the DMA (Peripheral and Memory DMA) view SHARC’s L1 memory?
  • Q&A
  • Files
  • Documents
  • Members
  • Tags
  • Cancel
  • +ADSP-SC57x/2157x: FAQ
  • +ADSP-SC58x: FAQ
  • +PMU registers: FAQ
  • +SC58x: FAQ
  • -SHARC+: FAQ
    • How many cycles does it take for a branch in SHARC+ ? How can I improve?
    • Does BTB affect the performance of the SHARC+ core when there is a branch misprediction?
    • Does hardware loops exist in SHARC+ Core ? Are they different from SHARC Core ?
    • How to handle Self modifying codes in SHARC+ Core?
    • In SHARC+ Core, does the external instruction fetch get cached in the Instruction Conflict Cache ?
    • In SHARC+ Core, for which interrupt does the status push happens automatically?
    • Is self-nesting of Interrupts allowed in SHARC+ Core?
    • Is Software Interrupt for Cortex A5 and SHARC core common?
    • Is the Core interrupt priority programmable in SHARC+ Core as in SHARC Core?
    • Is the Interrupt Vector table in SHARC+ core same as that in SHARC core?
    • Is there a scenario which results in a pipeline stall when the SHARC+ core is accessing L1 memory?
    • How does the DMA (Peripheral and Memory DMA) view SHARC’s L1 memory?
    • Is there any way that an Interrupt processing can be delayed in SHARC+ Core?
    • What is the difference between SHARC and SHARC+ Core pipeline?
    • What is the minimum latency between a Core interrupt and the branch to the IVT?
    • Are the branch operations impacted by the increase in the number of pipeline stages in SHARC+ Core? If so, how are they mitigated?
    • Are the CCES Run-time libraries optimized for SHARC+ Core?
    • Are the registers used to program the core interrupts in SHARC+ same as in SHARC Core?
    • Are there any new Core interrupts in SHARC+ Core?
    • Can all the core interrupts be masked in SHARC+ Core?
    • Is there any change in the L1 memory map of SHARC+ Core of ADSP-SC589when compared to SHARC Core in ADSP-214xx family of processors?
    • What are the different stages of pipeline in SHARC+ Core ?
    • What is the number of MAC operations that can be done in parallel in SHARC+ Core?
    • Where is the default IVT of SHARC+ Core located? Can it be changed?
    • Which L1 memory alias should the peripherals use to access the SHARC+ L1 Memory?
    • Will Boot streams generated for SPI master for SHARC+ core only boot on Power on Reset?
  • +TMU: FAQ
  • +215XX: FAQ
  • +ADC Control Module: FAQ
  • +ADSP-21584: FAQ
  • +ADSP-215xxl: FAQ
  • +ADSP-SC573: FAQ
  • +ADSP-SC5xx/215xx: FAQ
  • +ADSP-SC5xx: FAQ
  • +CCES default startup routine: FAQ
  • +EMAC: FAQ
  • +HADC: FAQ
  • +Hardware Counter based Loops: FAQ
  • +L1 block: FAQ
  • +Preload code customization: FAQ
  • +RDEN bit: FAQ
  • +RGMII/RMII: FAQ
  • +SHARC EE-377: FAQ
  • +Sharc SC584: FAQ
  • +SMMR using MDMA2: FAQ
  • +UCOS: FAQ
  • +USBCLKSEL in CGU_CLKOUT: FAQ
  • ADSP-21569 SPORT single-transmitter multi-receiver example
  • ADSP-SC584 SSL Booting via ROM API from the ARM Cortex A5 (core0), SHARC0 and SHARC1
  • +adsp-sc584: FAQ
  • ADSP-SC594 SPDIF Example
  • ADSP-SC835 SPI Slave transmitter and Master Receiver example code
  • Are code segments placed in block1 and block2, when data caches are enabled?
  • ASRC TDM8/TDM16 Example for ADSP-SC59x
  • Can we use internal pull down resistor for ADSP-SC59x/ADSP-2159x LP_CLK and LP_ACK pins instead of external pull down?
  • +CDU: FAQ
  • Custom Error Handler in Booting for SC594
  • DAI Interrupt example for ADSP-SC573
  • Do ADSP-SC58x/ADSP-SC57x support adi_pkte.h and adi_pka.h?
  • Does QUAD SPI open-drain mode need external pull-up resistors for each of these signals (MISO, MOSI, D2 & D3) in ADSP-21569
  • Does the LRCLK support 50% duty cycle in TDM mode?
  • Does the TMREXP(Timer Expired) pin support in latest SHARC processor?
  • Driver file support for the ADSP-SC584/SC589 custom board, which utilizes the same flash and DDR as Ez-kit.
  • Flash write example for ADSP-SC573 Ez-Kit
  • How many cycles for a cache hit/miss?
  • How many times the DAI can be routed using SRU?
  • How to configure DAI interrupt in ADSP-21569?
  • How to use Assembly to Control Core Flags?
  • How to use PCG trigger event
  • How to use PC_07 instead of SYS_FAULT in ADSP-2156x/ADSP-SC59x/ADSP-2159x ?
  • +IDLE: FAQ
  • Is it possible to change the sampling/driving edges of the ASRC?
  • Is it possible to configure the DSP as Master and Host as Slave once SPI slave booting done?
  • Is it possible to disable/halt/pause the SHARC0/SHARC1 cores from ARM core?
  • Is it possible to verify Secure Booting without programming Keys into OTP Memory?
  • Is the SPIx_RDY signal necessary for SPI slave boot?
  • JEDEC thermal Resistance Data estimation for "θJA, θJC, ΨJT" in ADSP-SC5xx/ADSP-215xx processor.
  • +Local Oscillator: FAQ
  • +MLB channels: FAQ
  • +MSI IDMAC: FAQ
  • Once the processor is locked, is it possible to debug or flash a new application?
  • +Program the CBS parameters: FAQ
  • +SC57x: FAQ
  • SCB arbitration/priority scheme
  • +Sign and encrypt a normal bootstream: FAQ
  • SPI example for ADSP-SC584
  • SPI secure slave boot
  • +SPORT with ACM: FAQ
  • +SWU: FAQ
  • Understanding Halt feature in ACM Mode
  • Usage of flush_data_buffer api
  • Using MCAPI/MDMA for ADSP-SC594 Dual-SHARC Audio Talkthrough
  • What is "Multiplexed Function Input Tap" available in the "Signal Multiplexing" table in the datasheet.
  • What is the clock configuration (HFCLK, BCLK) required to transmit SPDIF?
  • What is the difference between ENUM_DMA_CFG_XCNT_INT and ENUM_DMA_CFG_PERIPH_INT?
  • What is the recommended TMU_GAIN and TMU_OFFSET value for Calibration?
  • What is the SPORT Latency using DMA between the SHARC cores(Core1 & Core2) for ADSP-SC58x?
  • What is the supported SLCK0 divisor value for ADSP-2156x

How does the DMA (Peripheral and Memory DMA) view SHARC’s L1 memory?

All the DMA engines view SHARC’s L1 memory space from System View as Byte Addressable space.

For example SHARC0’s L1 Block 0 SRAM start address for a data byte access is 0x0024_0000.

In system view it corresponds to 0x2824_0000.

So the address passed to the DMA engine needs to be adjusted in the code by the user to take care of the Offset 0x2800_0000 for SHARC0’s core L1 internal memory.

Similarly for SHARC1’s L1 internal memory, an Offset of 0x2880_0000 needs to be passed to the DMA engine.