Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

EngineerZone
EngineerZone
ADSP-SC5xx/ADSP-215xx
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-SC5xx/ADSP-215xx
  • Processors & DSP
  • SHARC Processors
  • ADSP-SC5xx/ADSP-215xx
  • Cancel
ADSP-SC5xx/ADSP-215xx
Documents ASRC TDM8/TDM16 Example for ADSP-SC59x
  • Q&A
  • Files
  • Documents
  • Members
  • Tags
  • Cancel
  • +ADSP-SC57x/2157x: FAQ
  • +ADSP-SC58x: FAQ
  • +PMU registers: FAQ
  • +SC58x: FAQ
  • +SHARC+: FAQ
  • +TMU: FAQ
  • +215XX: FAQ
  • +ADC Control Module: FAQ
  • +ADSP-21584: FAQ
  • +ADSP-215xxl: FAQ
  • +ADSP-SC573: FAQ
  • +ADSP-SC5xx/215xx: FAQ
  • +ADSP-SC5xx: FAQ
  • +CCES default startup routine: FAQ
  • +EMAC: FAQ
  • +HADC: FAQ
  • +Hardware Counter based Loops: FAQ
  • +L1 block: FAQ
  • +Preload code customization: FAQ
  • +RDEN bit: FAQ
  • +RGMII/RMII: FAQ
  • +SHARC EE-377: FAQ
  • +Sharc SC584: FAQ
  • +SMMR using MDMA2: FAQ
  • +UCOS: FAQ
  • +USBCLKSEL in CGU_CLKOUT: FAQ
  • ADSP-21569 SPORT single-transmitter multi-receiver example
  • ADSP-SC584 SSL Booting via ROM API from the ARM Cortex A5 (core0), SHARC0 and SHARC1
  • +adsp-sc584: FAQ
  • ADSP-SC594 SPDIF Example
  • ADSP-SC835 SPI Slave transmitter and Master Receiver example code
  • Are code segments placed in block1 and block2, when data caches are enabled?
  • ASRC TDM8/TDM16 Example for ADSP-SC59x
  • Can we use internal pull down resistor for ADSP-SC59x/ADSP-2159x LP_CLK and LP_ACK pins instead of external pull down?
  • +CDU: FAQ
  • Custom Error Handler in Booting for SC594
  • DAI Interrupt example for ADSP-SC573
  • Do ADSP-SC58x/ADSP-SC57x support adi_pkte.h and adi_pka.h?
  • Does QUAD SPI open-drain mode need external pull-up resistors for each of these signals (MISO, MOSI, D2 & D3) in ADSP-21569
  • Does the LRCLK support 50% duty cycle in TDM mode?
  • Does the TMREXP(Timer Expired) pin support in latest SHARC processor?
  • Driver file support for the ADSP-SC584/SC589 custom board, which utilizes the same flash and DDR as Ez-kit.
  • Flash write example for ADSP-SC573 Ez-Kit
  • How many cycles for a cache hit/miss?
  • How many times the DAI can be routed using SRU?
  • How to configure DAI interrupt in ADSP-21569?
  • How to use Assembly to Control Core Flags?
  • How to use PCG trigger event
  • How to use PC_07 instead of SYS_FAULT in ADSP-2156x/ADSP-SC59x/ADSP-2159x ?
  • +IDLE: FAQ
  • Is it possible to change the sampling/driving edges of the ASRC?
  • Is it possible to configure the DSP as Master and Host as Slave once SPI slave booting done?
  • Is it possible to disable/halt/pause the SHARC0/SHARC1 cores from ARM core?
  • Is it possible to verify Secure Booting without programming Keys into OTP Memory?
  • Is the SPIx_RDY signal necessary for SPI slave boot?
  • JEDEC thermal Resistance Data estimation for "θJA, θJC, ΨJT" in ADSP-SC5xx/ADSP-215xx processor.
  • +Local Oscillator: FAQ
  • +MLB channels: FAQ
  • +MSI IDMAC: FAQ
  • Once the processor is locked, is it possible to debug or flash a new application?
  • +Program the CBS parameters: FAQ
  • +SC57x: FAQ
  • SCB arbitration/priority scheme
  • +Sign and encrypt a normal bootstream: FAQ
  • SPI example for ADSP-SC584
  • SPI secure slave boot
  • +SPORT with ACM: FAQ
  • +SWU: FAQ
  • Understanding Halt feature in ACM Mode
  • Usage of flush_data_buffer api
  • Using MCAPI/MDMA for ADSP-SC594 Dual-SHARC Audio Talkthrough
  • What is "Multiplexed Function Input Tap" available in the "Signal Multiplexing" table in the datasheet.
  • What is the clock configuration (HFCLK, BCLK) required to transmit SPDIF?
  • What is the difference between ENUM_DMA_CFG_XCNT_INT and ENUM_DMA_CFG_PERIPH_INT?
  • What is the recommended TMU_GAIN and TMU_OFFSET value for Calibration?
  • What is the SPORT Latency using DMA between the SHARC cores(Core1 & Core2) for ADSP-SC58x?
  • What is the supported SLCK0 divisor value for ADSP-2156x

ASRC TDM8/TDM16 Example for ADSP-SC59x

Attached is the ASRC example code in TDM8/TDM16 mode for ADSP-SC59x. Please comment/ uncomment the TDM mode in the "ASRC_TDM_Mode.h" as per the requirement.

As shown in the below figures, using the TDM output port several ASRCs can be daisy-chained together and connected to the SPORT of this or another processor. The ASRC OP contains a 64-bit parallel load shift register. When the SRCx_FS_OP_I pulse arrives, each ASRC loads its left and right data into the 64-bit shift register. The input to the shift register is connected to SRCx_TDM_OP_I, and the output is connected to SRCx_DAT_OP_O. By connecting the SRCx_DAT_OP_O to the SRCx_TDM_OP_I of the next ASRC, a large shift register is created, which is clocked by SRCx_CLK_OP_I.

If the ASRC is used in TDM8 mode, 4 ASRCs are daisy chained to create the TDM8 support. Similary, to acheive ASRC TDM16 mode, 8 ASRCs are daisy chained to create the TDM16 support.

Please refer the below figures for for TDM8 and TDM16.

TDM8:

TDM16:

SC594_ASRC_TDM8_TDM16.zip

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • FAQ : ASRC TDM8 example code for ADSP-2148x
    Sara Collins
    The ASRC can operate in TDM, I 2 S, left-justified, right-justified, and bypass modes. The serial ports of the processor can be used for moving the ASRC data to/from the internal memory. This example is...
  • RE: 21569 ASRC + TDM Questions
    ADIApproved
    Hi, Regarding 2, >>Each ASRC can support two channels, hence according to the number of channels present, we can daisy chain ASRC’s accordingly. For example, to support TDM16, 8 ASRC’s can be daisy chained...
  • RE: ASRC TDM Mode Example for EV-21569-EZKIT
    Divya.P
    Hi Norbert, Regarding"My understanding of four ASRCs used in daisy-chain is that they can be used to work on four independant stereo channels for upsampling or downsampling. Therefore, I would expect eight...
 
Related Content
  • FAQ : ASRC TDM8 example code for ADSP-2148x
    Sara Collins
    The ASRC can operate in TDM, I 2 S, left-justified, right-justified, and bypass modes. The serial ports of the processor can be used for moving the ASRC data to/from the internal memory. This example is...
  • RE: 21569 ASRC + TDM Questions
    ADIApproved
    Hi, Regarding 2, >>Each ASRC can support two channels, hence according to the number of channels present, we can daisy chain ASRC’s accordingly. For example, to support TDM16, 8 ASRC’s can be daisy chained...
  • RE: ASRC TDM Mode Example for EV-21569-EZKIT
    Divya.P
    Hi Norbert, Regarding"My understanding of four ASRCs used in daisy-chain is that they can be used to work on four independant stereo channels for upsampling or downsampling. Therefore, I would expect eight...