Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

EngineerZone
EngineerZone
ADSP-SC5xx/ADSP-215xx
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-SC5xx/ADSP-215xx
  • Processors & DSP
  • SHARC Processors
  • ADSP-SC5xx/ADSP-215xx
  • Cancel
ADSP-SC5xx/ADSP-215xx
Documents Usage of flush_data_buffer api
  • Q&A
  • Files
  • Documents
  • Members
  • Tags
  • Cancel
  • +ADSP-SC57x/2157x: FAQ
  • +ADSP-SC58x: FAQ
  • +PMU registers: FAQ
  • +SC58x: FAQ
  • +SHARC+: FAQ
  • +TMU: FAQ
  • +215XX: FAQ
  • +ADC Control Module: FAQ
  • +ADSP-21584: FAQ
  • +ADSP-215xxl: FAQ
  • +ADSP-SC573: FAQ
  • +ADSP-SC5xx/215xx: FAQ
  • +ADSP-SC5xx: FAQ
  • +CCES default startup routine: FAQ
  • +EMAC: FAQ
  • +HADC: FAQ
  • +Hardware Counter based Loops: FAQ
  • +L1 block: FAQ
  • +Preload code customization: FAQ
  • +RDEN bit: FAQ
  • +RGMII/RMII: FAQ
  • +SHARC EE-377: FAQ
  • +Sharc SC584: FAQ
  • +SMMR using MDMA2: FAQ
  • +UCOS: FAQ
  • +USBCLKSEL in CGU_CLKOUT: FAQ
  • ADSP-21569 SPORT single-transmitter multi-receiver example
  • ADSP-SC584 SSL Booting via ROM API from the ARM Cortex A5 (core0), SHARC0 and SHARC1
  • +adsp-sc584: FAQ
  • ADSP-SC594 SPDIF Example
  • ADSP-SC835 SPI Slave transmitter and Master Receiver example code
  • Are code segments placed in block1 and block2, when data caches are enabled?
  • ASRC TDM8/TDM16 Example for ADSP-SC59x
  • Can we use internal pull down resistor for ADSP-SC59x/ADSP-2159x LP_CLK and LP_ACK pins instead of external pull down?
  • +CDU: FAQ
  • Custom Error Handler in Booting for SC594
  • DAI Interrupt example for ADSP-SC573
  • Do ADSP-SC58x/ADSP-SC57x support adi_pkte.h and adi_pka.h?
  • Does QUAD SPI open-drain mode need external pull-up resistors for each of these signals (MISO, MOSI, D2 & D3) in ADSP-21569
  • Does the LRCLK support 50% duty cycle in TDM mode?
  • Does the TMREXP(Timer Expired) pin support in latest SHARC processor?
  • Driver file support for the ADSP-SC584/SC589 custom board, which utilizes the same flash and DDR as Ez-kit.
  • Flash write example for ADSP-SC573 Ez-Kit
  • How many cycles for a cache hit/miss?
  • How many times the DAI can be routed using SRU?
  • How to configure DAI interrupt in ADSP-21569?
  • How to use Assembly to Control Core Flags?
  • How to use PCG trigger event
  • How to use PC_07 instead of SYS_FAULT in ADSP-2156x/ADSP-SC59x/ADSP-2159x ?
  • +IDLE: FAQ
  • Is it possible to change the sampling/driving edges of the ASRC?
  • Is it possible to configure the DSP as Master and Host as Slave once SPI slave booting done?
  • Is it possible to disable/halt/pause the SHARC0/SHARC1 cores from ARM core?
  • Is it possible to verify Secure Booting without programming Keys into OTP Memory?
  • Is the SPIx_RDY signal necessary for SPI slave boot?
  • JEDEC thermal Resistance Data estimation for "θJA, θJC, ΨJT" in ADSP-SC5xx/ADSP-215xx processor.
  • +Local Oscillator: FAQ
  • +MLB channels: FAQ
  • +MSI IDMAC: FAQ
  • Once the processor is locked, is it possible to debug or flash a new application?
  • +Program the CBS parameters: FAQ
  • +SC57x: FAQ
  • SCB arbitration/priority scheme
  • +Sign and encrypt a normal bootstream: FAQ
  • SPI example for ADSP-SC584
  • SPI secure slave boot
  • +SPORT with ACM: FAQ
  • +SWU: FAQ
  • Understanding Halt feature in ACM Mode
  • Usage of flush_data_buffer api
  • Using MCAPI/MDMA for ADSP-SC594 Dual-SHARC Audio Talkthrough
  • What is "Multiplexed Function Input Tap" available in the "Signal Multiplexing" table in the datasheet.
  • What is the clock configuration (HFCLK, BCLK) required to transmit SPDIF?
  • What is the difference between ENUM_DMA_CFG_XCNT_INT and ENUM_DMA_CFG_PERIPH_INT?
  • What is the recommended TMU_GAIN and TMU_OFFSET value for Calibration?
  • What is the SPORT Latency using DMA between the SHARC cores(Core1 & Core2) for ADSP-SC58x?
  • What is the supported SLCK0 divisor value for ADSP-2156x

Usage of flush_data_buffer api

The assembler supports the following instructions related to flushing the cache:
FLUSH <CACHE(s)>  
WRITEBACK <CACHE(s)>
INVALIDATE <CACHE(s)>   

flush_invalidate_caches() – uses “FLUSH DM_CACHE & FLUSH PM_CACHE ” instruction.
This instruction ensures that the cache is cleared and any updated copy in the cache is not cleared without writing back to L2/L3 memory.

flush_no_invalidate_caches() – uses “WRITEBACK DM_CACHE & WRITEBACK PM_CACHE” instruction: This instruction ensures that all the modified data in cache is written back to L2/L3. But it will not clear the cache.

"INVALIDATE DM_CACHE & INVALIDATE PM_CACHE" instruction clears the cache unconditionally without writing back to L2/L3 memory.

flush_data_buffer api with ADI_FLUSH_DATA_INV,  calls flush_invalidate_caches() which Invalidates *and* writes back the specified caches(s).
flush_data_buffer api with ADI_FLUSH_DATA_NOINV, calls flush_no_invalidate_caches() which Writes back the specified caches(s).

If your input data buffer resides in cacheable memory, then after modifying the buffer it should be flushed from memory using the flush_data_buffer API in the ADI_FLUSH_DATA_NOINV mode. This prevents the DMA transfer from accessing stale data.

If your results buffer resides in cacheable memory, then before triggering the RX DMA channel to permit transferring new results, the buffer should be flushed using the flush_data_buffer API in the ADI_FLUSH_DATA_NOINV mode. The data should then not be accessed until the RX DMA channel says the next set of results are ready. When the results are ready, the buffer should be invalidated by calling the flush_data_buffer API in the ADI_FLUSH_DATA_INV mode.