Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
ADSP-SC5xx/ADSP-215xx
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-SC5xx/ADSP-215xx
  • Processors & DSP
  • SHARC Processors
  • ADSP-SC5xx/ADSP-215xx
  • Cancel
ADSP-SC5xx/ADSP-215xx
Documents ADSP-SC584 SSL Booting via ROM API from the ARM Cortex A5 (core0), SHARC0 and SHARC1
  • Q&A
  • Files
  • Documents
  • Members
  • Tags
  • Cancel
  • +ADSP-SC57x/2157x: FAQ
  • +ADSP-SC58x: FAQ
  • +PMU registers: FAQ
  • +SC58x: FAQ
  • +SHARC+: FAQ
  • +TMU: FAQ
  • +215XX: FAQ
  • +ADC Control Module: FAQ
  • +ADSP-21584: FAQ
  • +ADSP-215xxl: FAQ
  • +ADSP-SC573: FAQ
  • +ADSP-SC5xx/215xx: FAQ
  • +ADSP-SC5xx: FAQ
  • +CCES default startup routine: FAQ
  • +EMAC: FAQ
  • +HADC: FAQ
  • +Hardware Counter based Loops: FAQ
  • +L1 block: FAQ
  • +Preload code customization: FAQ
  • +RDEN bit: FAQ
  • +RGMII/RMII: FAQ
  • +SHARC EE-377: FAQ
  • +Sharc SC584: FAQ
  • +SMMR using MDMA2: FAQ
  • +UCOS: FAQ
  • +USBCLKSEL in CGU_CLKOUT: FAQ
  • ADSP-21569 SPORT single-transmitter multi-receiver example
  • ADSP-SC584 SSL Booting via ROM API from the ARM Cortex A5 (core0), SHARC0 and SHARC1
  • +adsp-sc584: FAQ
  • ADSP-SC594 SPDIF Example
  • ADSP-SC835 SPI Slave transmitter and Master Receiver example code
  • Are code segments placed in block1 and block2, when data caches are enabled?
  • ASRC TDM8/TDM16 Example for ADSP-SC59x
  • Can we use internal pull down resistor for ADSP-SC59x/ADSP-2159x LP_CLK and LP_ACK pins instead of external pull down?
  • +CDU: FAQ
  • Custom Error Handler in Booting for SC594
  • DAI Interrupt example for ADSP-SC573
  • Do ADSP-SC58x/ADSP-SC57x support adi_pkte.h and adi_pka.h?
  • Does QUAD SPI open-drain mode need external pull-up resistors for each of these signals (MISO, MOSI, D2 & D3) in ADSP-21569
  • Does the LRCLK support 50% duty cycle in TDM mode?
  • Does the TMREXP(Timer Expired) pin support in latest SHARC processor?
  • Driver file support for the ADSP-SC584/SC589 custom board, which utilizes the same flash and DDR as Ez-kit.
  • Flash write example for ADSP-SC573 Ez-Kit
  • How many cycles for a cache hit/miss?
  • How many times the DAI can be routed using SRU?
  • How to configure DAI interrupt in ADSP-21569?
  • How to use Assembly to Control Core Flags?
  • How to use PCG trigger event
  • How to use PC_07 instead of SYS_FAULT in ADSP-2156x/ADSP-SC59x/ADSP-2159x ?
  • +IDLE: FAQ
  • Is it possible to change the sampling/driving edges of the ASRC?
  • Is it possible to configure the DSP as Master and Host as Slave once SPI slave booting done?
  • Is it possible to disable/halt/pause the SHARC0/SHARC1 cores from ARM core?
  • Is it possible to verify Secure Booting without programming Keys into OTP Memory?
  • Is the SPIx_RDY signal necessary for SPI slave boot?
  • JEDEC thermal Resistance Data estimation for "θJA, θJC, ΨJT" in ADSP-SC5xx/ADSP-215xx processor.
  • +Local Oscillator: FAQ
  • +MLB channels: FAQ
  • +MSI IDMAC: FAQ
  • Once the processor is locked, is it possible to debug or flash a new application?
  • +Program the CBS parameters: FAQ
  • +SC57x: FAQ
  • SCB arbitration/priority scheme
  • +Sign and encrypt a normal bootstream: FAQ
  • SPI example for ADSP-SC584
  • SPI secure slave boot
  • +SPORT with ACM: FAQ
  • +SWU: FAQ
  • Understanding Halt feature in ACM Mode
  • Usage of flush_data_buffer api
  • Using MCAPI/MDMA for ADSP-SC594 Dual-SHARC Audio Talkthrough
  • What is "Multiplexed Function Input Tap" available in the "Signal Multiplexing" table in the datasheet.
  • What is the clock configuration (HFCLK, BCLK) required to transmit SPDIF?
  • What is the difference between ENUM_DMA_CFG_XCNT_INT and ENUM_DMA_CFG_PERIPH_INT?
  • What is the recommended TMU_GAIN and TMU_OFFSET value for Calibration?
  • What is the SPORT Latency using DMA between the SHARC cores(Core1 & Core2) for ADSP-SC58x?
  • What is the supported SLCK0 divisor value for ADSP-2156x

ADSP-SC584 SSL Booting via ROM API from the ARM Cortex A5 (core0), SHARC0 and SHARC1

An SSL is a stand-alone application that is executed at boot time before the actual application is dynamically loaded into memory. The SSL can be used to invoke a ROM API to boot a second application.
The ROM API can be accessed at runtime by any core to boot an application from a boot source, but booting via the API is completely different as compared with POR, as it depends on which core is calling it:

Case 1 ->If the ROM API is invoked from the ARM Cortex A5 (core0), then the boot kernel can boot applications to all three cores.

Case 2 ->If the ROM API is invoked from the primary SHARC (core1), then the boot kernel can boot applications to both SHARC cores (core1 and core2), but not to the ARM (core0).

Case 3 ->If the ROM API is invoked from the secondary SHARC (core2), then the boot kernel can only boot the core2 SHARC (not the core 0 ARM nor the core1 SHARC).

Attached project demonstrates booting of ADSP-SC584 cores when the ROM API is invoked from the ARM Cortex A5 (core0), SHARC0 and SHARC1 named as Case1, Case2 and Case3.

Attached folder contains two projects namely SC584_SSL and SC584_LED. The SC584_SSL project invokes ROM API(first booting application). The SC584_LED is the second booting application.

Along with these projects, the loader streams are also attached.

ADSP_SC584_SSL_Allcases.zip

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: ADSP-SC587 adi_rom_boot() for Second Stage Load
    ADIApproved
    Hello, As this query is closed in the private support, post the final resolution for others to get benefit. Seems that you call the adi_rom_boot function from SHARC core 2. In that case, as mentioned...
  • RE: SC58x boot from ROM (or Flash?)
    Harshit.Gaharwar
    Hi, When you are calling a ROM API to boot a second application from first application, then you need to make sure that there is no memory conflict between the two applications. Once this is done,...
  • Will Boot streams generated for SPI master for SHARC+ core only boot on Power on Reset?
    Sara Collins
    In terms of the Boot flow, in ADSP-SC58x, Cortex A5 is the primary core which does all the memory initialization and comes out of Reset on Power On reset. The other two SHARC+ cores remains in reset and...
 
Related Content
  • RE: ADSP-SC587 adi_rom_boot() for Second Stage Load
    ADIApproved
    Hello, As this query is closed in the private support, post the final resolution for others to get benefit. Seems that you call the adi_rom_boot function from SHARC core 2. In that case, as mentioned...
  • RE: SC58x boot from ROM (or Flash?)
    Harshit.Gaharwar
    Hi, When you are calling a ROM API to boot a second application from first application, then you need to make sure that there is no memory conflict between the two applications. Once this is done,...
  • Will Boot streams generated for SPI master for SHARC+ core only boot on Power on Reset?
    Sara Collins
    In terms of the Boot flow, in ADSP-SC58x, Cortex A5 is the primary core which does all the memory initialization and comes out of Reset on Power On reset. The other two SHARC+ cores remains in reset and...