Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Dont Let Your Feedback Loop Fall FlatPart 2: Dynamic Response and Isolation Innovation!

    Introduction In isolated power supply systems, maintaining a stable output voltage under varying load conditions is essential for reliable operation. The...

EngineerZone
EngineerZone
ADSP-SC5xx/ADSP-215xx
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-SC5xx/ADSP-215xx
  • Processors & DSP
  • SHARC Processors
  • ADSP-SC5xx/ADSP-215xx
  • Cancel
ADSP-SC5xx/ADSP-215xx
Documents ADSP-SC58x: FAQ
  • Q&A
  • Files
  • Documents
  • Members
  • Tags
  • Cancel
  • +ADSP-SC57x/2157x: FAQ
  • -ADSP-SC58x: FAQ
    • ADSP-SC58x FMU(Fault Management Unit) Example Code.
    • ADSP-SC58x SPI Quad example code
    • ADSP-SC58X How to configure EMDMA Gather mode
    • ADSP-SC58x/2158x ACM- Example code
    • How to configure GIC of edge triggered interrupt sources?
    • ADSP-SC58x/2158x ASRC:Example codes
    • ADSP-SC58x/2158x Cortex A5 Software Interrupt- Example code
    • How to enable only L1 cache and not L2 cache OR vice-versa?
    • ADSP-SC58x/2158x Counter: Example code
    • How to extend number of channels in HADC
    • ADSP-SC58x/2158x DAI : What's new?
    • ADSP-SC58x/2158x interrupt SHARC core from ARM:Example code
    • How to select PSIZE and MSIZE fields of the MDMA configuration register on ADSP-SC58x/ADSP-2158x ?
    • ADSP-SC58x/2158x L2 access restriction from MDMA using SMPU - Example code
    • ADSP-SC58x/2158x Multicore: Example Code
    • ADSP-SC58x/2158x OTP General Purpose space programming- Example code
    • ADSP-SC58x/2158x PCG : Example codes
    • ADSP-SC58x/2158x PKA ECC multiplication  - Example code
    • Is it possible to change the default boot mode peripheral instances?
    • ADSP-SC58x/2158x PKTE Encryption - Example code
    • Is it possible to run a DDR2 device at DCLK=400 MHz, CCLK=450 MHz, SYSCLK=225Mz on ADSP-SC58x/ADSP-2158x processors?
    • ADSP-SC58x/2158x PKTE Encryption-Hashing  - Example code
    • Is it possible to run all the accelerators FIR/IIR/FFT in ADSP-SC58x/ADSP-2158x simultaneously?
    • ADSP-SC58x/2158x PKTE Hashing-Decryption  - Example code
    • Is Secure booting supported in Open part in ADSP-SC58x?
    • ADSP-SC58x/2158x PWM: What's new?
    • ADSP-SC58x/2158x SPDIF-RX feature list: What's new?
    • ADSP-SC58x/2158x SPDIF: Example code
    • ADSP-SC58x/2158x SPI - Example Code
    • +ADSP-SC58x/2158x SPI XIP - Example code
    • ADSP-SC58x/2158x TRNG - Example code
    • ADSP-SC58x/2158x UART autobaud - Code Example
    • ADSP-SC58x/2158x Watchdog Timer:Example code
    • Is there a way to slow down the compute engine of the FFTA on ADSP-SC58x/ADSP-2158x processor?
    • ADSP-SC58x/ADSP-215xx SHARC+ Core Timer with Interrupt Example Code
    • Is there any L2 cache in ADSP-SC58x?
    • How can I validate the DDR interface on my newely designed board based on ADSP-SC58x/ADSP-2158x processors?
    • ADSP-SC5xx/ADSP-215xx - DDR memory Test
    • Is there any restriction on the types of memories supported by MDMA on ADSP-SC58x/ADSP-2158x?
    • How can the high speed FFTA DMA engine on ADSP-SC58x/ADSP-2158x be used in MDMA mode?
    • Highlights of MSI on ADSP-SC58x
    • Is there anything equivalent to External Port DMA (EPDMA) on ADSP-214xx processors available on ADSP-SC58x/ADSP-2158x processors?
    • How FIR accelerator on ADSP-SC58x/ADSP-2158x is different than the FIR accelerator on ADSP-214xx?
    • Is VFP and Neon available in ADSP-SC58x?
    • How FFT accelertor on ADSP-SC58x/ADSP-2158x can be programmed?
    • How many CRC blocks available on ADSP-SC58x/ADSP-2158x processor ?
    • How is SWU on SC58x different from that on BF60x processor?
    • How is the ACM on SC58x different from that on BF60x processor?
    • What should I do to SYS_CLKIN1 on SC58x, if I need only one CLKIN in my system
    • Can ARM Cortex A5 access SHARC core internal memory space in ADSP-SC58x?
    • Can FIR accelerator access both on chip and off chip memories on ADSP-SC58x/ADSP-2158x processor?
    • Secure Slave boot modes fails to boot even after programming the correct Public and Private key in the OTP space in ADSP-SC58x. What else is missing?
    • What are the major changes in the programming model of the IIR accelerator on ADSP-SC58x/ADSP-2158x as compared to ADSP-214xx processors?
    • What all Boot modes are supported in ADSP-SC58x?
    • What are the major differences in between the programming model of DDR3, DDR2, and LPDDR modes in the DMC controller of ADSP-SC58x/ADSP-2158x?
    • What are the major features of the CRC engine on ADSP-SC58x/ADSP-2158x processors?
    • what's new in the SPI peripheral of SC58x processor?
    • Can I connect DDR3 memory device on one DMC and DDR2 memory device on another DMC on ADSP-SC58x/ADSP-2158x?
    • Can I use the MLB Clock on SC58x to clock an external system?
    • What DDR3/DDR2/LPDDR device sizes are supported by the DMC controller on ADSP-SC58x/ADSP-2158x?
    • Can IIR accelerator access both on chip and off chip memories on ADSP-SC58x/ADSP-2158x?
    • Can Performance Monitor Unit be used to calculate cycle counts for SHARC core?
    • What is maximum speed of operation supported by Link Port in ADSP-SC58x?
    • Can the CRC engine on ADSP-SC58x/ADSP-2158x be used to calculate 16 bit CRC ?
    • What is Oscillator Watchdog?
    • Can the existing SHARC assembly codes be re-used as it is with SHARC+ Core?
    • Can we single-step over the IDLE instruction?
    • What is the maximum DMA throughput supported by L2CTL memory system on ADSP-SC58x/ADSP-2158x processors?
    • Do both the SHARC+ Cores in ADSP-SC58x/ADSP-215xx share the same L1 Memory?
    • What is the maximum processing speed supported by Cortex-A5 in ADSP-SC58x?
    • Does MDMA support descriptor based DMAs on ADSP-SC58x/ADSP-2158x?
    • What is the maximum speed supported by the MLB interface on SC58x?
    • What is Multiprocessor Offset in ADSPSC58x/ADSP-215xx processors??
    • What is the minimum DCLK frequency supported for various DDR modes on ADSP-SC58x/ADSP-2158x?
    • I have configured my MDMA on ADSP-SC58x correctly, but still the MDMA transfer doesn't work as expected. Am I missing something?
    • How many MDMA streams are supported by ADSP-SC58x/ADSP-2158x processors and how much bandwidth they support?
    • What is the size if L1 cache supported by Cortex A5 in ADSP-SC58x?
    • FIRA/IIRA Performance on ADSP-SC58x/2158x and ADSP-SC57x/2157x Processors
    • How DMC/DDR controller in ADSP-SC58x/ADSP-2158x different than DDR2 controller on ADSP-2146x ?
    • I installed the IIR DMA interrupt handler on ADSP-SC58x, but still the interrupt doesn't occur, what I may be missing?
    • In ADSP-SC58x, can the ARM core access the SHARC+ Core's L1 Memory?
    • What are the important features of the L2 memory system on ADSP-SC58x/ADSP-2158x processors?
    • What are the major changes in the programming model of the FIR accelerator on ADSP-SC58x/ADSP-2158x as compared to ADSP-214xx processors?
    • How does the ECC error protection on L2 memory system works on ADSP-SC58x/ADSP-2158x processors?
    • How can I run the core clock at maximum of 450MHz and also source a 125MHz at the CLK07 for the EMAC TXCLK?
    • How does the memory refresh operation in L2CTL memory system works on ADSP-SC58x/ADSP-2158x processors?
    • How FFT accelerator (FFTA) on ADSP-SC58x/ADSP-2158x is different as compared to ADSP-214xx processors / What are the major features of FFTA on ADSP-SC58x/ADSP-2158x ?
    • How IIR accelerator on ADSP-SC58x/ADSP-2158x is different than the FIR accelerator on ADSP-214xx?
    • How is GP Timer in SC57x/2157x different from that of SC58x?
    • How is the MLB interface on SC58x different from previous SHARC processors?
    • How is the SPI peripheral different from the older SHARC processors?
    • How many DMC controllers are present in ADSP-SC58x/ADSP-2158x processors?
    • How many instances of EMAC are present in SC58x? How are they different?
    • How the FIR and IIR accelerators in ADSP-SC57x/2157x processors are different than in ADSP-SC58x/2158x processors
    • ADSP-SC584 SPORT Core mode example
    • ADSP-SC58x Multicore SPORT TDM example
    • ADSP-SC58x/2158x PMU Overflow Interrupt- Example code
    • ADSP-SC58x/ADSP-2158x Linkport Example code
    • Code Example: UART 0,1 and 2 communication across two ADSP-SC589 Ez-Kits
    • EPPI Peripheral on ADSP-SC589
    • What will be the state of GPIO pins during reset for ADSP-SC589?
  • +PMU registers: FAQ
  • +SC58x: FAQ
  • +SHARC+: FAQ
  • +TMU: FAQ
  • +215XX: FAQ
  • +ADC Control Module: FAQ
  • +ADSP-21584: FAQ
  • +ADSP-215xxl: FAQ
  • +ADSP-SC573: FAQ
  • +ADSP-SC5xx/215xx: FAQ
  • +ADSP-SC5xx: FAQ
  • +CCES default startup routine: FAQ
  • +EMAC: FAQ
  • +HADC: FAQ
  • +Hardware Counter based Loops: FAQ
  • +L1 block: FAQ
  • +Preload code customization: FAQ
  • +RDEN bit: FAQ
  • +RGMII/RMII: FAQ
  • +SHARC EE-377: FAQ
  • +Sharc SC584: FAQ
  • +SMMR using MDMA2: FAQ
  • +UCOS: FAQ
  • +USBCLKSEL in CGU_CLKOUT: FAQ
  • ADSP-21569 SPORT single-transmitter multi-receiver example
  • ADSP-SC584 SSL Booting via ROM API from the ARM Cortex A5 (core0), SHARC0 and SHARC1
  • +adsp-sc584: FAQ
  • ADSP-SC594 SPDIF Example
  • ADSP-SC835 SPI Slave transmitter and Master Receiver example code
  • Are code segments placed in block1 and block2, when data caches are enabled?
  • ASRC TDM8/TDM16 Example for ADSP-SC59x
  • Can we use internal pull down resistor for ADSP-SC59x/ADSP-2159x LP_CLK and LP_ACK pins instead of external pull down?
  • +CDU: FAQ
  • Custom Error Handler in Booting for SC594
  • DAI Interrupt example for ADSP-SC573
  • Do ADSP-SC58x/ADSP-SC57x support adi_pkte.h and adi_pka.h?
  • Does QUAD SPI open-drain mode need external pull-up resistors for each of these signals (MISO, MOSI, D2 & D3) in ADSP-21569
  • Does the LRCLK support 50% duty cycle in TDM mode?
  • Does the TMREXP(Timer Expired) pin support in latest SHARC processor?
  • Driver file support for the ADSP-SC584/SC589 custom board, which utilizes the same flash and DDR as Ez-kit.
  • Flash write example for ADSP-SC573 Ez-Kit
  • How many cycles for a cache hit/miss?
  • How many times the DAI can be routed using SRU?
  • How to configure DAI interrupt in ADSP-21569?
  • How to use Assembly to Control Core Flags?
  • How to use PCG trigger event
  • How to use PC_07 instead of SYS_FAULT in ADSP-2156x/ADSP-SC59x/ADSP-2159x ?
  • +IDLE: FAQ
  • Is it possible to change the sampling/driving edges of the ASRC?
  • Is it possible to configure the DSP as Master and Host as Slave once SPI slave booting done?
  • Is it possible to disable/halt/pause the SHARC0/SHARC1 cores from ARM core?
  • Is it possible to verify Secure Booting without programming Keys into OTP Memory?
  • Is the SPIx_RDY signal necessary for SPI slave boot?
  • JEDEC thermal Resistance Data estimation for "θJA, θJC, ΨJT" in ADSP-SC5xx/ADSP-215xx processor.
  • +Local Oscillator: FAQ
  • +MLB channels: FAQ
  • +MSI IDMAC: FAQ
  • Once the processor is locked, is it possible to debug or flash a new application?
  • +Program the CBS parameters: FAQ
  • +SC57x: FAQ
  • SCB arbitration/priority scheme
  • +Sign and encrypt a normal bootstream: FAQ
  • SPI example for ADSP-SC584
  • SPI secure slave boot
  • +SPORT with ACM: FAQ
  • +SWU: FAQ
  • Understanding Halt feature in ACM Mode
  • Usage of flush_data_buffer api
  • Using MCAPI/MDMA for ADSP-SC594 Dual-SHARC Audio Talkthrough
  • What is "Multiplexed Function Input Tap" available in the "Signal Multiplexing" table in the datasheet.
  • What is the clock configuration (HFCLK, BCLK) required to transmit SPDIF?
  • What is the difference between ENUM_DMA_CFG_XCNT_INT and ENUM_DMA_CFG_PERIPH_INT?
  • What is the recommended TMU_GAIN and TMU_OFFSET value for Calibration?
  • What is the SPORT Latency using DMA between the SHARC cores(Core1 & Core2) for ADSP-SC58x?
  • What is the supported SLCK0 divisor value for ADSP-2156x

ADSP-SC58x: FAQ

Attached is the ADSP-SC58x example code for firmware upgrade via UART along with multiple loader streams. Also the attached ADSP-SC58x_UART_Firmware_Upgrade.pdf document contains the procedure to upgrade the firmware.
PDF
7127.UART_Firmware_Upgrade.zip