Post Go back to editing

ADSP-SC58x/2158x Simple Led- Example code for Boot Testing

Attached folder comprises of a simple LED blink code for all the 3 cores in ADSP-SC58x processor. Apart from that it also has a loader stream generated for SPI master boot mode for various combination.

These loader streams can be programmed into the flash and SPI master boot can be tested.

Boot_Code.zip
Parents
  • Hi,

    I used the code on ADSP-SC58x_EZ-KIT and it seemed to be flashed on the DSP and running.

    The only thing I could not get it verify that it is working properly or not is that I could not get this development board LEDs (LED10 or 11 or 12) to blink using this code.

    The board manual says these LEDs are for PE_13, PE_14 and PE_15 but I do not find a reference for these pins to modify the code you attached. I want to know how I can modify the code you attached in order to get these LEDs on the EVAL-SC589-EZLITE kit blinking?

    Thanks

Reply
  • Hi,

    I used the code on ADSP-SC58x_EZ-KIT and it seemed to be flashed on the DSP and running.

    The only thing I could not get it verify that it is working properly or not is that I could not get this development board LEDs (LED10 or 11 or 12) to blink using this code.

    The board manual says these LEDs are for PE_13, PE_14 and PE_15 but I do not find a reference for these pins to modify the code you attached. I want to know how I can modify the code you attached in order to get these LEDs on the EVAL-SC589-EZLITE kit blinking?

    Thanks

Children
No Data