Problem with compiling SC589 power on self test in CCES 2.1.0

I've downloaded the CCES 2.1.0.0 (w1508281) on my computer.

I received the SC589 eval kit.

I try to compile the power on self test from the BSP "ADSP-SC58x_EZ-KIT_Lite-Rel1.0.0"

I try to compile the power on self test, but I get errors on the ethernet driver.

In the linking process I got undifined references from the file common/source/ethernet_test.c for the functions:

adi_ether_Open, adi_ether_SetMACAddress, adi_ether_EnableMAC, adi_ether_GetLinkStatus, adi_ether_Read, adi_ether_Write and adi_ether_Close

I got other missing references from the file ina3221_test.c to the functions adi_ina3221_Open,adi_ina3221_ConfigTWI, adi_ina3221_ReadManufacturerID, adi_ina3221_ReadDieID, adi_ina3221_Reset, adi_ina3221_Close

Is this a known issue, and am I using some wrong version (BSP or CCES) ?

If so, where can I find the latest releases of the software ?

Thanks in advance,

Br,

Thierry

  • I found out that not all neede drivers are linked in the project file.

    It is solved by adding the missing ethernet drivers from the CCES driver path, and the ADC drivers from the EZ-kit Board support package path.

    This can be done in the project, properties.  In the recoursec > linked resources the needed drivers can be linked.  Make sure only to link them, and not load them as files.

    The missing drivers where eg. CCES\ARM\arm-none-eabi\arm-none-eabi\lib\src\cortex-a5\drivers\Source\ethernet\gemac\adi_gemac_pps_alarm.c

    I've found all drivers with a textual search.

    Br,

    Thierry

  • This question has been closed by the EZ team and is assumed answered.