How do I configure the SRU file for the SC584 EZ KIT EVM board

I am using the ADSP-SC584 EZ-Board.

I want to add the ADAU1977 to the Throughput project that basically uses the adau1979 and adau1962

I have 2 SRU_config files from the 2 different projects: Throughput project using the adau1979 + adau1962, and chan_freq example project using the adau1977.

I cant understand from the manual how to do the changes, even if I use the SRU files help does not come

The differences between the files are in the file attached

Maccabi

SRU_DAIdiffs.docx
Parents Reply Children