Post Go back to editing

Spec Related

Category: Datasheet/Specs
Product Number: ADZS SC589

Dear Team ,

This query is almost the same as Query 2 from the link below 

 RE: ADSP-SC589 Spec Questions 

Can anyone confirm if the SPDIF Rx supports 192kHz sampling Fs or not .

If yes can you please give me an example code(for CGU /CDU) that configures CLK05 for 225MHz

From HRM

Sample rates of 32 kHz to 192 kHz are supported using a 225.0 MHz setting on CLKO5.

How to set the condition above ? Any example code would be helpful 

Regards,

Hermione