Post Go back to editing

SC573 Ezkit CAN/MMC pin conflict

Category: Hardware
Product Number: SC573

The Linux documentation states: "For ADSP-SC573 Ezkit, Users should additionally disable the MMC support from Linux Kernel menuconfig due to pin conflict. Please refer to Mobile Storage Interface for MMC/SD."

(1) Does this mean that neither CAN interface can be used in an application that also uses the MMC/SD card? I need the higher speed one (TJA1145).

(2) Is this a limitation only with Linux, or also with bare metal applications?

(3) Are there any more details about exactly what the "pin conflict" is, i.e. which peripheral/signal? Both SD and CAN are required for my evaluation, I don't mind hacking the board if I need to.

Many thanks in advance. 

Thread Notes

Parents Reply Children
No Data