Post Go back to editing

In the case of multiple firmwares, how to get the current firmware address of the SPI flash when running the main() function?

Category: Software
Product Number: ADSP-21593
Software Version: 2.11.1.0(w2210191)

Hi .

I'm currently design the second-stage-loader(SSL)  and when a new firmware stored in SPI flash chip, SSL will first call adi_rom_Boot() function to test the new firmware before cover the old one(the one stored at the beginning address of SPI flash)

so here is the question: is there a way to get the current firmware address of the SPI flash ?

greatly appreciate for your help!