Post Go back to editing

How many channels can be used when SPORTs is Multichannel (TDM) mode

How many channels can be used when SPORT configure as TDM mode,The maximum channels is 128 or 1024?

when two sports use the same Channel Select,is there any poblem? Do they conflict?

/*! Specifies the SPORT0A Channel Select 0 register Configuration*/
#define ADI_SPORT_0A_CS0 0xfful
/*! Specifies the SPORT0A Channel Select 1 register Configuration*/
#define ADI_SPORT_0A_CS1 0x00ul
/*! Specifies the SPORT0A Channel Select 2 register Configuration*/
#define ADI_SPORT_0A_CS2 0x00ul
/*! Specifies the SPORT0A Channel Select 3 register Configuration*/
#define ADI_SPORT_0A_CS3 0x00ul

/* Specifies the SPORT0B Channel Select 0 register Configuration*/
#define ADI_SPORT_0B_CS0 0xfful
/* Specifies the SPORT0B Channel Select 1 register Configuration*/
#define ADI_SPORT_0B_CS1 0x00ul
/* Specifies the SPORT0B Channel Select 2 register Configuration*/
#define ADI_SPORT_0B_CS2 0x00ul
/* Specifies the SPORT0B Channel Select 3 register Configuration*/
#define ADI_SPORT_0B_CS3 0x00ul

Parents Reply Children
No Data