Hi,
I have some problems when using SPDIF driver and I asked in another post, but I get no answer. So I start a new post here.
I need to use both SPDIF Tx and Rx, and I use another device made by ADAU1452 which is pretty good in both Tx an Rx to test the 21565 SPDIF driver.
Here are my tests. All the Tx send to Rx is using AES connector through a cable outside.
1. I use 21565 SPDIF Tx send to 21565 Rx, it's good work.
2. I use 1452 SPDIF Tx send to 1452 Rx, it's good work.
3. I use 1452 SPDIF Tx send to 21565 Rx, it's good work.
4. I use 21565 SPDIF Tx send to 1452 Rx, there's no audio received in 1452.
5. I enable the standalone mode in 21565 Tx and then I use 21565 SPDIF Tx send to 1452 Rx, I can get audios in 1452.
My question is why 21565 Tx can't send to another device unless when enable standalone mode?
Thanks!